cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103ZE Flash interface

allenpoper
Associate II
Posted on February 28, 2014 at 12:15

Hello,

   I am plan make custom board with STM32F103ZE chip. My question is, what is the interface for flashing the program in to flash?is it USART(UART)? or JTAG?
10 REPLIES 10
chen
Associate II
Posted on February 28, 2014 at 15:17

Hi

We use the SWD method. We have ST-Link V2

http://www.st.com/web/en/catalog/tools/FM146/CL1984/SC724/SS1677/PF251168

http://uk.farnell.com/stmicroelectronics/st-link-v2/icd-programmer-for-stm8-stm32/dp/1892523

The programs we use is

St-Lin Util (just handles the .hex)

http://www.st.com/web/en/catalog/tools/PF258168

We also use an IDE debugger but I would not recommend the one we use (Atollic) - it is terrible.

Go for IAR or Keil or GreenHills

In addition, my job was to develop our own custom bootloader which runs over USB CDC