cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103Z Timer Problem

samed
Associate II
Posted on November 18, 2013 at 17:43

I have a Timer Problem . I want that my timer every 1ms makes an interrupt .

I testes it here if (TIM2_Tick >= 1000) but my LED was alway on then I tryied

if (TIM2_Tick >= 1000000) and it was about 1 sec (30 blinks in 34 sec)

My system_clk is 72Mhz .

where is my mistake

void Config_Timer(TIM_TimeBaseInitTypeDef *TIM_TimeBaseStructure, NVIC_InitTypeDef *NVIC_InitStructure)

{

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

    

 /* Enable the Timer2 Interrupt */

  NVIC_InitStructure->NVIC_IRQChannel = TIM2_IRQn;                          //  configure the Timer2 interrupts

  NVIC_InitStructure->NVIC_IRQChannelPreemptionPriority = 0;   //  sets the priority group of the TIMER2 interrupts

  NVIC_InitStructure->NVIC_IRQChannelSubPriority = 1;                    //  set the subpriority inside the group

  NVIC_InitStructure->NVIC_IRQChannelCmd = ENABLE;                            //  TIMER2 interrupts are globally enabled

  NVIC_Init(NVIC_InitStructure);        

    

    /* Configure Timer which is every 1 ms active*/

  TIM_DeInit(TIM2);

  TIM_TimeBaseStructInit(TIM_TimeBaseStructure);

 

  /* Time base configuration */

  TIM_TimeBaseStructure->TIM_Prescaler = 360 - 1; // 72 MHz / 360 = 200 khz

  TIM_TimeBaseStructure->TIM_Period = 200 - 1;    // (1/200khz) * 200 = 1 ms;

  TIM_TimeBaseStructure->TIM_ClockDivision = 0;

  TIM_TimeBaseStructure->TIM_CounterMode = TIM_CounterMode_Up;

  TIM_TimeBaseInit(TIM2, TIM_TimeBaseStructure);

    

 

    

  /* Enable TIM2 Update Interrupt */

  TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);

 

  /* Enable TIM2 */

  TIM_Cmd(TIM2,ENABLE);

         

}

void TIM2_IRQHandler(void)

{

    static int TIM2_Tick = 0; 

      

     TIM2_Tick++;

        if (TIM2_Tick >= 1000) // 1 Second

                {

                    if(check == 0)

                    {

                        STM_EVAL_LEDOn(LED1);

                        check=1;

                    }

                    else

                    {

                        STM_EVAL_LEDOff(LED1);

                        check =0;

                    }

                    

                    TIM2_Tick = 0;

        }

}

I set check=0 in my main once

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on November 18, 2013 at 18:00

You don't clear the interrupt, the routine will keep re-entering.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
samed
Associate II
Posted on November 19, 2013 at 11:06

You mean

TIM_ClearITPendingBit

(

TIM2

,

TIM_IT_Update

)

;

in my TIM2_IRQHandler ?

I put it inside and now the LED is blinking  by the condition if (TIM2_Tick >= 1000)

frequent but not like a second . More about 10 times in 19 sec

Posted on November 19, 2013 at 13:33

I put it inside and now the LED is blinking  by the condition if (TIM2_Tick >= 1000) frequent but not like a second. More about 10 times in 19 sec.

But you understand that if you toggle a pin you effectively half the frequency, right?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
samed
Associate II
Posted on November 19, 2013 at 14:32

mhh not really maybe you can tell me my mistake.

I thought that every 1ms  my TIM2_IRQHandler is called. Right ?

Because of the if if (TIM2_Tick >= 1000) it enters only in when my tick is over 1000. right ?

I thought when I toogle my LED It will not take about 0,5 s right ?
Posted on November 19, 2013 at 15:52

For a PERIOD of 1000 ms, the duty for the HIGH and LOW will be 500 ms each, NOT 1000

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..