cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103VFT6 99CBK 93 A MYS 99 322

FLast.14
Associate III

Hi 

 

Since almost 10 years I'm working with STM32F103VF microcontroller with KEIL IDE, and I don't have any problem. But yesterday I received the last batch from my PCB manufacturer, and it installs that reference STM32F103VFT6 as always, but I can't debug with KEIL. And I don't understand why. 

 

I erased all sectors, and with ST-link Utility I can program my device successfully, but I can't debug with KEIL. 

 

Is anything to take into account to debug it? 

If I check the completely name writted in the microcontroller I can see: STM32F103VFT6 99CBK 93 A MYS 99 322

Is this batch the problem?

 

Regards, 

12 REPLIES 12
FLast.14
Associate III

Now, I'm doing test with STM32CubeIDE with the same microcontroller and I cann't debug either. When I start debug, after 1-2seconds the program stops debugging and I can't jump to any breakpoint, and no errors are appearing.
If I test with other ST microcontroller batch, all is working fine.

Hi @FLast.14 ,

can you provide the UniqueID dump registers and also the package top marking , we need first to know if it is a genuine STM32F1.

Cheers,

STOne-32

The UniqueID is: 

FLast14_0-1707999300387.png

 

The top marking of the pill is:

FLast14_1-1707999469266.png

The top marking of the package I don't have know here because I sent to my PCB manufacturer. I bought these microcontrollers in Official ST Distributor.