2011-06-25 10:59 AM
Hey
people
,
Recently
I bought
the STM32F103RBT6 development board + 2.8'' TFT-module
. (A.k.a MINI-STM32-V3.0) (with the 2 mini USBs)
After many
attempts
to enter
programming
mode
,
and
program it
via
USB without any extra tools
,
I managed
.
i used this combination to enter the programing mode: (PRESS and HOLD the BOOT0 key, Press and Release the RESET key, Release the BOOT0 key) i used the PL2303 Driver to set my ''USB to Serial'' Virtual COM and i used the ''Flash Loader Demo'' to upload the example code to my board.The program
worked
and
everything was good
...
but
When
I tried
againto enter
programming
mode
(in order to change the code),
the
STM32F103RBT6
stuck
on the
programming
mode
(
white
screen
).
i tried to program it (in the same way i managed before) but nothing, Now, when ever i power up my board i see a white screen, the four keys (RESET, BOOT0, KEY1, KEY2) doesn't respond and the''Flash Loader Demo''
application cannot communicate with the board.
I am really afraid that somehow my board hasBricked\Spoiled
.
I willAppreciate any help in this subject, thanks
#metoo #lmgtfy2013-02-22 05:34 AM
Hi,
I'm in the same situation as you. Did you find out how to proceed without the CD? I've contacted my seller and am awaiting a response. Lets hope.2013-02-22 10:11 AM
Like this one?
With schematics and sample code to download? Or this Perhaps you can link to the specific one you are talking about?