Question
Triggering ADC from Timer. Does timer output have to be enabled?
Posted on January 04, 2013 at 16:31
Hi,
I'm using a STM32F103. My main question is, is there a way to trigger an ADC regular group using a timer output compare channel but without enabling output to the timer channel's physical output pin? I've been trying to trigger ADC1 with TIM4_CH4, but I have to use the default pin for TIM4_CH4 for I2C1 and I can't remap TIM4_CH4 because that pin is used for external RAM. I started with the example code posted in ''Timer4 trigger for ADC'' (Posted: 6/15/2011 4:44 PM) and that works fine. But, if I remap I2C1 (using the default TIM4_CH4 pin), the timer interferes with the I2C. And, if I disable the timer's output, (TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Disable), the ADC does not get triggered. Is it just that you can't trigger an ADC without using the timer's output pin or does it seem like I have something else messed up? Below is the example code from ''Timer4 trigger for ADC''. Thanks.TIM4_CC4 should be viable (TIMER 4 CHANNEL 4)
You'll need to program ADC1->CR2, with EXTSEL[2:0] = 5 (101)/* TIM4 configuration ------------------------------------------------------*/
/* Time Base configuration */ TIM_TimeBaseStructInit(&TIM_TimeBaseStructure); TIM_TimeBaseStructure.TIM_Period = 0xFF; TIM_TimeBaseStructure.TIM_Prescaler = 0x4; TIM_TimeBaseStructure.TIM_ClockDivision = 0x0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure); /* TIM4 channel4 configuration in PWM mode */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 0x7F; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low; TIM_OC4Init(TIM4, &TIM_OCInitStructure);..
/* ADC1 configuration ------------------------------------------------------*/
ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T4_CC4; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfChannel = 1; ADC_Init(ADC1, &ADC_InitStructure); #adc-tim