STM32F103C8T6 USART wrong data
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-10-23 03:29 AM
Hello,
I have a problem with sending data from/to my STM32F103C8T6 using USART connection. I'm using USB2TTL PL2303 converter. I connected it to RX1 and TX1 on the board. I can send .hex files with STM Flash Loader Demonstrator and it works (like LED blink etc.). This is how it looks like:http://image.prntscr.com/image/0d03529e29c64d78b6c3fb08bbaf57f8.png
http://image.prntscr.com/image/0d03529e29c64d78b6c3fb08bbaf57f8.png
This is my code:
void
startUsart(){
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA,
ENABLE
);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,
ENABLE
);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO,
ENABLE
);
GPIO_InitTypeDef
GPIO_InitStructure;
GPIO_InitStructure.
GPIO_Pin
= GPIO_Pin_9;
GPIO_InitStructure.
GPIO_Mode
=
GPIO_Mode_AF_PP
;
GPIO_InitStructure.
GPIO_Speed
=
GPIO_Speed_50MHz
;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.
GPIO_Pin
= GPIO_Pin_10;
GPIO_InitStructure.
GPIO_Mode
=
GPIO_Mode_IN_FLOATING
;
GPIO_Init(GPIOA, &GPIO_InitStructure);
USART_InitTypeDef
uart;
uart.
USART_BaudRate
= 115200;
uart.
USART_HardwareFlowControl
= USART_HardwareFlowControl_None;
uart.
USART_Mode
= USART_Mode_Rx | USART_Mode_Tx;
uart.
USART_Parity
= USART_Parity_No;
uart.
USART_StopBits
= USART_StopBits_1;
uart.
USART_WordLength
= USART_WordLength_8b;
USART_Init(USART1, &uart);
USART_Cmd(USART1,
ENABLE
);
}
void
send_char(
char
c)
{
while
(USART_GetFlagStatus(USART1, USART_FLAG_TXE) ==
RESET
);
USART_SendData(USART1, c);
}
int
main(
int
argc,
char
* argv[])
{
startUsart();
while
(1)
{
send_char(
'y'
);
timer_sleep(2000);
send_char(
'a'
);
timer_sleep(2000);
}
}
What I receive is:
http://image.prntscr.com/image/4c508ec85ff9476f99689ce8e1a5epng
I was looking for similar problem but couldn’t find any working solution.
I tried lower baudrate like 9600 but still not working.
stm32 usart stm32f103- Labels:
-
STM32F1 Series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-10-23 06:00 AM
You'd need to review HSE_VALUE used for the project vs whatever crystal your board uses. You could try just using the HSI clock rather than the HSE/PLL
Suggest you output a U characters, and look at the TX signal on a scope to verify/understand the bit clock it is using.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-10-23 08:57 AM
My HSE_VALUE = 8000000.
I generated code with STM32Cube for this task and it works (characters received from the board are correct). I can see that there is the same HSE_VALUE. I would prefer to have my own code rather than generated though but I'm note sure what to change in my project. Any tips?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-10-23 10:53 AM
Code doesn't look unreasonable, not sure of the tool chain used or if SystemInit is called. I'd scope the pin and review the clocks.
Up vote any posts that you find helpful, it shows what's working..