cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103C8T6 interface with 0.96 ST7735 LCD

mylim
Associate

Hi, I bought a module of STM32F103C8T6 with a 0.96" LCD. 

I managed to find the LCD library in Keil MDK. 

However, I am checking of anyone has successfully ported to STM32cubeIDE?

Thanks.

 

picture.jpg

 

 

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @mylim, to the community!

Your board is a so-called Blue Pill, which is neither an product of STMicroelectronics nor contains an microcontroller of STMicroelectronics. For years, only counterfeits have been installed there, so the STM32CubeIDE cannot support this.

There are plenty of original boards from STMicroelectronics that you can work with and which are of course supported, e.g. the NUCLEO-32.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.