cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103: Using DMA1 Channel 3 for SPI1_TX and USART3_RX same time

cfrpg
Associate

I'm currently working on a project using an STM32F103RET microcontroller. I need to use SPI1 to write log data to a flash chip at an rate of 64 bytes every 20 milliseconds, and use USART3 monitoring external communication, receiving an average of 30 bytes every 10 milliseconds. To minimizing CPU usage, I'm trying use DMA to handle data transmission, and find that SPI1_TX and USART3_RX share a same DMA channel (DMA1,channel 3).

The question is, is it possible to use DMA1 Channel 3 for both SPI1_TX and USART3_RX simultaneously on an STM32F103?

(My code runing in main loop without RTOS)

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

Unfortunately it’s not possible. Need to select another USART or SPI instance.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
waclawek.jan
Super User

No.

JW

mƎALLEm
ST Employee

Hello,

Unfortunately it’s not possible. Need to select another USART or SPI instance.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.