2017-08-01 2:56 AM
Hi all,
I've a problem on STM32F103RET6 microcontroller using the UART1 flow control in combination with the Bluegiga BT121 bluetooth chip. I'm using a custom board with these simple hardware configuration:
I'm using UART1 with DMA and this is the source code:
static
void
MX_USART1_UART_Init
(
void
)
{huart1
.
Instance
=
USART1
;
huart1
.
Init
.
BaudRate
=
460800
;
huart1
.
Init
.
WordLength
=
UART_WORDLENGTH_8B
;
huart1
.
Init
.
StopBits
=
UART_STOPBITS_1
;
huart1
.
Init
.
Parity
=
UART_PARITY_NONE
;
huart1
.
Init
.
Mode
=
UART_MODE_TX_RX
;
huart1
.
Init
.
HwFlowCtl
=
UART_HWCONTROL_RTS_CTS;
huart1
.
Init
.
OverSampling
=
UART_OVERSAMPLING_16
;
if
(
HAL_UART_Init
(
&
huart1
)
!=
HAL_OK
)
{
_Error_Handler
(
__FILE__
,
__LINE__
);
}
}void
HAL_UART_MspInit
(
UART_HandleTypeDef
*
huart
)
{
GPIO_InitTypeDef
GPIO_InitStruct
;
if
(
huart
->
Instance
==
USART1
)
{
/* Peripheral clock enable */
__HAL_RCC_USART1_CLK_ENABLE
();
/**USART1 GPIO Configuration
PA9 ------> USART1_TXP
PA10 ------> USART1_RX
PA11 ------> USART1_CTS
PA12 ------> USART1_RTS
*/
GPIO_InitStruct
.
Pin
=
GPIO_PIN_9
|
GPIO_PIN_12
;
GPIO_InitStruct
.
Mode
=
GPIO_MODE_AF_PP
;
GPIO_InitStruct
.
Speed
=
GPIO_SPEED_FREQ_HIGH
;
HAL_GPIO_Init
(
GPIOA
,
&
GPIO_InitStruct
);
GPIO_InitStruct
.
Pin
=
GPIO_PIN_10
|
GPIO_PIN_11
;
GPIO_InitStruct
.
Mode
=
GPIO_MODE_INPUT
;
GPIO_InitStruct
.
Pull
=
GPIO_NOPULL
;
HAL_GPIO_Init
(
GPIOA
,
&
GPIO_InitStruct
);
/* USART1 DMA Init */
/* USART1_TX Init */
hdma_usart1_tx
.
Instance
=
DMA1_Channel4
;
hdma_usart1_tx
.
Init
.
Direction
=
DMA_MEMORY_TO_PERIPH
;
hdma_usart1_tx
.
Init
.
PeriphInc
=
DMA_PINC_DISABLE
;
hdma_usart1_tx
.
Init
.
MemInc
=
DMA_MINC_ENABLE
;
hdma_usart1_tx
.
Init
.
PeriphDataAlignment
=
DMA_PDATAALIGN_BYTE
;
hdma_usart1_tx
.
Init
.
MemDataAlignment
=
DMA_MDATAALIGN_BYTE;
hdma_usart1_tx
.
Init
.
Mode
=
DMA_NORMAL
;
hdma_usart1_tx
.
Init
.
Priority
=
DMA_PRIORITY_VERY_HIGH
;
if
(
HAL_DMA_Init
(
&
hdma_usart1_tx
)
!=
HAL_OK
)
{
_Error_Handler
(
__FILE__
,
__LINE__
)}
}
__HAL_LINKDMA
(
huart
,
hdmatx
,
hdma_usart1_tx
);
/* USART1_RX Init */
hdma_usart1_rx
.
Instance
=
DMA1_Channel5
;
hdma_usart1_rx
.
Init
.
Direction
=
DMA_PERIPH_TO_MEMORY
;
hdma_usart1_rx
.
Init
.
PeriphInc
=
DMA_PINC_DISABLE
;
hdma_usart1_rx
.
Init
.
MemInc
=
DMA_MINC_ENABLE
;
hdma_usart1_rx
.
Init
.
PeriphDataAlignment
=
DMA_PDATAALIGN_BYTE
;
hdma_usart1_rx
.
Init
.
MemDataAlignment
=
DMA_MDATAALIGN_BYTE
;
hdma_usart1_rx
.
Init
.
Mode
=
DMA_CIRCULAR
;
hdma_usart1_rx
.
Init
.
Priority
=
DMA_PRIORITY_VERY_HIGH
;
if
(
HAL_DMA_Init
(
&
hdma_usart1_rx
)
!=
HAL_OK
)
{
_Error_Handler
(
__FILE__
,
__LINE__
);
}
__HAL_LINKDMA
(
huart
,
hdmarx
,
hdma_usart1_rx
);
/* USART1 interrupt Init */
HAL_NVIC_SetPriority
(
USART1_IRQn
,
0
,
0
);
HAL_NVIC_EnableIRQ
(
USART1_IRQn
);
}
}
The problem is that
I can only send data but not receive
!I did several tests:
1. add pull-up resistors2. change the transmission speed3. try with a different hardware: ST Inemo + BT121 evaluation board but the only solution I found to be able to send messages was to disable the flow control.So, my question is: d
oes anyone have any idea why it does not work?
What am I doing wrong?
Many thanks in advance
#stm32f103 #flow-control #bluetooth #uart2017-08-01 4:29 AM
Hello!!
Your BAUD RATE is not correct. (
huart1
.
Init
.
BaudRate
=
460800
)(not default)
2017-08-01 6:35 AM
Hi Vangelis,
I also tried lower baud rates, for example 115200, 9600, without any positive result
2017-08-01 8:05 AM
Hello again.
Trannsmission speed must be 115200
all commands send to module must be consistent to BGAPI.
In
DMA Mode RX , try to use circular mode DMA .
2017-08-01 9:23 AM
Hello Vangelis,
DMA RX mode is already circular and also setting baudrate at 115200 it doesn't work.
I'm not using BGAPI, but this BGscript:
&sharpvariable definitions dim rep
dim f, p ♯ Boot event listener - Generated when the module is startedevent system_boot(major,minor,patch,build,bootloader,hw) rep=-1 call endpoint_set_streaming_destination(0,31)endevent system_initialized(addr) call system_set_local_name(4,'TEST') call bt_rfcomm_start_server(2,0) call bt_gap_set_mode(1,1,0) call le_gap_set_mode(0,0) call sm_configure(0,3) call sm_set_bondable_mode(1)endevent endpoint_status(endpoint,type,destination,flags) if (type = endpoint_rfcomm) && (flags&ENDPOINT_FLAG_ACTIVE) call bt_gap_set_mode(0,1,0) rep=endpoint call endpoint_send(0,15,'CONNECTED') call endpoint_set_streaming_destination(0,endpoint) end ifendevent endpoint_closing(reason,endpoint) call bt_gap_set_mode(1,1,0) call endpoint_close(endpoint) if(endpoint = rep) call endpoint_send(0,18,'DISCONNECTED') end ifendevent le_connection_closed(reason,connection) call le_gap_set_mode(0,0)endIn your opinion, is it possible a flow control incompatibility between ST microcontroller and BT121?
2017-08-01 11:59 AM
IMHO i think there is not flow control incompatibility. (SILABS recomends this setup)
I don't know how this script is compiled as compatible ARM code to your device.
Read
andhttp://community.silabs.com/t5/Bluetooth-Wi-Fi-Knowledge-Base/Programming-the-BT121/ta-p/173579
from silabs. Contains valuable information for your setup.2017-08-02 8:15 AM
Hi Vangelis,
I also found that documentation but it was not helpful for me to solve the problem.
But I did a strange discovery: if instead of UART1 I use the UART2 of the microcontroller, then communication works correctly even in reception!
How is it possible?
I only changed all references from UART1 to UART2