Skip to main content
Carlo Agrusti
Associate II
April 24, 2017
Question

STM32F103 SPI configuration troubles

  • April 24, 2017
  • 2 replies
  • 1219 views
Posted on April 24, 2017 at 18:18

Hi all,

I'm having hard times in configuring SPI communication with a M95128 eeprom; I'm using SPI1 on a STM32F103 mcu, with following connection scheme:

PA.04 -> ~S (CS)

PA.05 -> C (CLK)

PA.06 -> Q (MISO)

PA.07 -> D (MOSI)

and here follows my configuration code snippet:

/*
 * enable APB2 peripheral clock for SPI1
 */
 RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);
 RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE);
/*
 * configure pins used for SPI1
 * PA.04 = CS
 * PA.05 = SCK
 * PA.06 = MISO (Master In/Slave Out)
 * PA.07 = MOSI (Master Out/Slave In)
 */
 GPIO_InitStruct.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_5;
 GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF_PP;
 GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;
 GPIO_Init(GPIOA, &GPIO_InitStruct);
 GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6;
 GPIO_InitStruct.GPIO_Mode = GPIO_Mode_IN_FLOATING;
 GPIO_Init(GPIOA, &GPIO_InitStruct);
/*
 * The MISO, MOSI and CLK pins are now connected to their AF
 * so that the SPI1 can take over control of the pins
 */
 GPIO_PinLockConfig(GPIOA, GPIO_Pin_5);
 GPIO_PinLockConfig(GPIOA, GPIO_Pin_6);
 GPIO_PinLockConfig(GPIOA, GPIO_Pin_7);
/*
 * configure CS (PA.04) as output Open Drain
 */
 GPIO_InitStruct.GPIO_Pin = GPIO_Pin_4;
 GPIO_InitStruct.GPIO_Mode = GPIO_Mode_Out_OD;
 GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;
 GPIO_Init(GPIOA, &GPIO_InitStruct);
 GPIOA->BSRR = GPIO_Pin_4; // set CS (PA.04) high
/*
 * configure SPI1 in Mode 0
 * CPOL = 0 --> clock is low when idle
 * CPHA = 0 --> data is sampled at the first edge
 */
 SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex; // set to full duplex mode, seperate MOSI and MISO lines
 SPI_InitStruct.SPI_Mode = SPI_Mode_Master; // transmit in master mode, NSS pin has to be always high
 SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b; // one packet of data is 8 bits wide
 SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low; // clock is low when idle
 SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge; // data sampled at first edge
 SPI_InitStruct.SPI_NSS = SPI_NSS_Soft; // set the NSS management to internal and pull internal NSS high
 SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256; // SPI frequency is APB2 frequency / 16 (4.5MHz)
 SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB; // data is transmitted MSB first
 SPI_Init(SPI1, &SPI_InitStruct);
 SPI_Cmd(SPI1, ENABLE); // enable SPI1
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

When I try to send a read status register instruction to the eeprom, I can see that the CLK correctly sends 8 pulses while the MOSI line stays stuck at 1, as shown by attached picture, thus resulting in a 0xFF sent to the eeprom instead of 0x05 (which is the opcode for read status register).

Any hint?

TIA,

CArlo

    This topic has been closed for replies.

    2 replies

    waclawek.jan
    Super User
    April 25, 2017
    Posted on April 25, 2017 at 13:33

    Can you toggle that pin manually, when set as GPIO Output?

    JW

    Carlo Agrusti
    Associate II
    April 26, 2017
    Posted on April 26, 2017 at 13:15

    Yes, I can drive PA.04 as CS for my M95128 eeprom