cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 I2C Busy flag

Manuel Forcen Munoz
Associate II
Posted on May 22, 2018 at 18:44

Hi to all.

I'm trying to use I2C peripheral of STM32F103C8T6. I'm using a BluePill board. First of all, I know that this problem was published in other forums and so, but after trying other solutions, I didn't find the way to make it work.

I'm using the last STM32CubeMX firmware 1.6.1 V for STM32F103C8Tx.

I tried to make an example that uses I2C in order to make a library for an SSD1306 I2C display.

The example consists of this:

  while (1)

  {

    HAL_GPIO_TogglePin(GPIOC, 1<<13);

    HAL_Delay(1000);

  /* USER CODE END WHILE */

      uint8_t buf = 0;

    volatile HAL_StatusTypeDef status;

    status = HAL_I2C_Master_Transmit(&hi2c1, 0x3c<<1, &buf,1, 100);

    HAL_I2C_IsDeviceReady(&hi2c1, 0x3c<<1, 100,200);

    try_unlock_i2c();

    status = HAL_I2C_Master_Transmit(&hi2c1, 0x3c<<1, &buf,1,100);

    HAL_I2C_ClearBusyFlagErrata_2_14_7(&hi2c1);

  /* USER CODE BEGIN 3 */

  }

Here, I call HAL_I2C_Master_Transmit function while the device is connected to the display, just in order to see the wave in a logic analyzer and in the debugger, but the fact is that no wave is shown.

Just to make sure the program was running, I launched the debugger and I read the status variable. With this, I saw that the function is returning HAL_BUSY. It happens to me almost every time I use the I2C peripheral.

I did my research, and I know about the errata thing, so I tried to implement some solutions I found on the Internet in order to clear the BUSY flag.

Please find attached my code.

I'm still learning this amazing microcontroller, so it may be a 'basic' thing.

Thanks in advance.

EDIT: Well, this is very strange, but right now it started to work properly. If anyone knows a possible reason, a reply would be appreciated, because it can happen another time.

#i2c #stm32f1 #stm32f103 #i2c-dma #busy #errata #ssd1306 #i2c-busy #busy-flag
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Can't help you, bumping you off my feed

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..