cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 HAL UART Receive Interrupt not working

AOuse.1
Associate

Hi,

I am using STM32F103 controller UART peripheral for serial communication.Using interrupt for receiving data. I am able to send data but not receiving any data using UART interrupt handler. Once the function entered inside the interrupt handler getting HAL_UART_BUSY status inside the UART_Receive_IT function. Once it received an interrupt then it is not going back to the main and continuously running inside the interrupt handler and getting Overrun error. Please let me know what are the issues and how I can solve it.

/**
  * @brief  Initializes the UART mode according to the specified parameters in
  *         the UART_InitTypeDef and create the associated handle.
  * @param  huart  Pointer to a UART_HandleTypeDef structure that contains
  *                the configuration information for the specified UART module.
  * @retval HAL status
  */
HAL_StatusTypeDef HAL_UART_Init(UART_HandleTypeDef *huart)
{
  /* Check the UART handle allocation */
  if (huart == NULL)
  {
    return HAL_ERROR;
  }
 
  /* Check the parameters */
  if (huart->Init.HwFlowCtl != UART_HWCONTROL_NONE)
  {
    /* The hardware flow control is available only for USART1, USART2 and USART3 */
    assert_param(IS_UART_HWFLOW_INSTANCE(huart->Instance));
    assert_param(IS_UART_HARDWARE_FLOW_CONTROL(huart->Init.HwFlowCtl));
  }
  else
  {
    assert_param(IS_UART_INSTANCE(huart->Instance));
  }
  assert_param(IS_UART_WORD_LENGTH(huart->Init.WordLength));
#if defined(USART_CR1_OVER8)
  assert_param(IS_UART_OVERSAMPLING(huart->Init.OverSampling));
#endif /* USART_CR1_OVER8 */
 
  if (huart->gState == HAL_UART_STATE_RESET)
  {
    /* Allocate lock resource and initialize it */
    huart->Lock = HAL_UNLOCKED;
 
#if (USE_HAL_UART_REGISTER_CALLBACKS == 1)
    UART_InitCallbacksToDefault(huart);
 
    if (huart->MspInitCallback == NULL)
    {
      huart->MspInitCallback = HAL_UART_MspInit;
    }
 
    /* Init the low level hardware */
    huart->MspInitCallback(huart);
#else
    /* Init the low level hardware : GPIO, CLOCK */
    HAL_UART_MspInit(huart);                  //ENABLE THE INTTERUPTS
#endif /* (USE_HAL_UART_REGISTER_CALLBACKS) */
  }
 
  huart->gState = HAL_UART_STATE_BUSY;
 
  /* Disable the peripheral */
  __HAL_UART_DISABLE(huart);
 
  /* Set the UART Communication parameters */
  UART_SetConfig(huart);
 
  /* In asynchronous mode, the following bits must be kept cleared:
     - LINEN and CLKEN bits in the USART_CR2 register,
     - SCEN, HDSEL and IREN  bits in the USART_CR3 register.*/
  CLEAR_BIT(huart->Instance->CR2, (USART_CR2_LINEN | USART_CR2_CLKEN));
  CLEAR_BIT(huart->Instance->CR3, (USART_CR3_SCEN | USART_CR3_HDSEL | USART_CR3_IREN));
 
  /* Enable the peripheral */
  __HAL_UART_ENABLE(huart);
 
  /* Initialize the UART state */
  huart->ErrorCode = HAL_UART_ERROR_NONE;
  huart->gState = HAL_UART_STATE_READY;
  huart->RxState = HAL_UART_STATE_READY;
 
  return HAL_OK;
}

The code attached below

/**
  * @brief  This function handles UART interrupt request.
  * @param  huart  Pointer to a UART_HandleTypeDef structure that contains
  *                the configuration information for the specified UART module.
  * @retval None
  */
void HAL_UART_IRQHandler(UART_HandleTypeDef *huart)
{
  uint32_t isrflags   = READ_REG(huart->Instance->SR);
  uint32_t cr1its     = READ_REG(huart->Instance->CR1);
  uint32_t cr3its     = READ_REG(huart->Instance->CR3);
  uint32_t errorflags = 0x00U;
  uint32_t dmarequest = 0x00U;
  /* If no error occurs */
  errorflags = (isrflags & (uint32_t)(USART_SR_PE | USART_SR_FE | USART_SR_ORE | USART_SR_NE));
  if (errorflags == RESET)
  {
    /* UART in mode Receiver -------------------------------------------------*/
    if (((isrflags & USART_SR_RXNE) != RESET) && ((cr1its & USART_CR1_RXNEIE) != RESET))
    {
		  __HAL_UART_CLEAR_FLAG(huart,UART_FLAG_RXNE);
      UART_Receive_IT(huart);
      return;
    }
  }
 
  /* If some errors occur */
  if ((errorflags != RESET) && (((cr3its & USART_CR3_EIE) != RESET) || ((cr1its & (USART_CR1_RXNEIE | USART_CR1_PEIE)) != RESET)))
  {
    /* UART parity error interrupt occurred ----------------------------------*/
    if (((isrflags & USART_SR_PE) != RESET) && ((cr1its & USART_CR1_PEIE) != RESET))
    {
      huart->ErrorCode |= HAL_UART_ERROR_PE;
    }
 
    /* UART noise error interrupt occurred -----------------------------------*/
    if (((isrflags & USART_SR_NE) != RESET) && ((cr3its & USART_CR3_EIE) != RESET))
    {
      huart->ErrorCode |= HAL_UART_ERROR_NE;
    }
 
    /* UART frame error interrupt occurred -----------------------------------*/
    if (((isrflags & USART_SR_FE) != RESET) && ((cr3its & USART_CR3_EIE) != RESET))
    {
      huart->ErrorCode |= HAL_UART_ERROR_FE;
    }
 
    /* UART Over-Run interrupt occurred --------------------------------------*/
    if (((isrflags & USART_SR_ORE) != RESET) && ((cr3its & USART_CR3_EIE) != RESET))
    {
      huart->ErrorCode |= HAL_UART_ERROR_ORE;
    }
 
    /* Call UART Error Call back function if need be --------------------------*/
    if (huart->ErrorCode != HAL_UART_ERROR_NONE)
    {
      /* UART in mode Receiver -----------------------------------------------*/
      if (((isrflags & USART_SR_RXNE) != RESET) && ((cr1its & USART_CR1_RXNEIE) != RESET))
      {
        UART_Receive_IT(huart);
      }
 
      /* If Overrun error occurs, or if any error occurs in DMA mode reception,
         consider error as blocking */
      dmarequest = HAL_IS_BIT_SET(huart->Instance->CR3, USART_CR3_DMAR);
      if (((huart->ErrorCode & HAL_UART_ERROR_ORE) != RESET) || dmarequest)
      {
        /* Blocking error : transfer is aborted
           Set the UART state ready to be able to start again the process,
           Disable Rx Interrupts, and disable Rx DMA request, if ongoing */
        UART_EndRxTransfer(huart);
 
        /* Disable the UART DMA Rx request if enabled */
        if (HAL_IS_BIT_SET(huart->Instance->CR3, USART_CR3_DMAR))
        {
          CLEAR_BIT(huart->Instance->CR3, USART_CR3_DMAR);
 
          /* Abort the UART DMA Rx channel */
          if (huart->hdmarx != NULL)
          {
            /* Set the UART DMA Abort callback :
               will lead to call HAL_UART_ErrorCallback() at end of DMA abort procedure */
            huart->hdmarx->XferAbortCallback = UART_DMAAbortOnError;
            if (HAL_DMA_Abort_IT(huart->hdmarx) != HAL_OK)
            {
              /* Call Directly XferAbortCallback function in case of error */
              huart->hdmarx->XferAbortCallback(huart->hdmarx);
            }
          }
          else
          {
            /* Call user error callback */
#if (USE_HAL_UART_REGISTER_CALLBACKS == 1)
            /*Call registered error callback*/
            huart->ErrorCallback(huart);
#else
            /*Call legacy weak error callback*/
            HAL_UART_ErrorCallback(huart);
#endif /* USE_HAL_UART_REGISTER_CALLBACKS */
          }
        }
        else
        {
          /* Call user error callback */
#if (USE_HAL_UART_REGISTER_CALLBACKS == 1)
          /*Call registered error callback*/
          huart->ErrorCallback(huart);
#else
          /*Call legacy weak error callback*/
          HAL_UART_ErrorCallback(huart);
#endif /* USE_HAL_UART_REGISTER_CALLBACKS */
        }
      }
      else
      {
        /* Non Blocking error : transfer could go on.
           Error is notified to user through user error callback */
#if (USE_HAL_UART_REGISTER_CALLBACKS == 1)
        /*Call registered error callback*/
        huart->ErrorCallback(huart);
#else
        /*Call legacy weak error callback*/
        HAL_UART_ErrorCallback(huart);
#endif /* USE_HAL_UART_REGISTER_CALLBACKS */
 
        huart->ErrorCode = HAL_UART_ERROR_NONE;
      }
    }
    return;
  } /* End if some error occurs */
 
  /* UART in mode Transmitter ------------------------------------------------*/
  if (((isrflags & USART_SR_TXE) != RESET) && ((cr1its & USART_CR1_TXEIE) != RESET))
  {
    UART_Transmit_IT(huart);
    return;
  }
 
  /* UART in mode Transmitter end --------------------------------------------*/
  if (((isrflags & USART_SR_TC) != RESET) && ((cr1its & USART_CR1_TCIE) != RESET))
  {
    UART_EndTransmit_IT(huart);
    return;
  }
}
/**
  * @brief This function handles USART1 global interrupt.
  */
void USART1_IRQHandler(void)
{
  /* USER CODE BEGIN USART1_IRQn 0 */
 
  /* USER CODE END USART1_IRQn 0 */
  HAL_UART_IRQHandler(&huart1);
  /* USER CODE BEGIN USART1_IRQn 1 */
 
  /* USER CODE END USART1_IRQn 1 */
}

Thank you,

Alphy

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

Your callback routine does what?​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
JArau.2
Associate

resolved?

waclawek.jan
Super User

Please start a new thread, clearly stating what is your problem, what hardware are you using, what are the symptoms, etc.

JW