cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f100: how start TIM1 interrupt handler

Posted on June 23, 2011 at 18:03

Hi!

I've to program STM32f100R4H6; particularly i've to manage TIM1 interrupt.

Below there is my code..Thank you in advance..

--------------------------------------------------------------------------------------------

//In the first part of the main..

void RCC_init(void){

// 1. Clocking the controller from internal HSI RC (8 MHz)

  RCC_HSICmd(ENABLE);

  // wait until the HSI is ready

  while(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET);

  RCC_SYSCLKConfig(RCC_SYSCLKSource_HSI);

  // 2. Enable ext. high frequency OSC

  RCC_HSEConfig(RCC_HSE_ON);

  // wait until the HSE is ready

  // 3. Init PLL

  RCC_PLLCmd(ENABLE);

  // wait until the PLL is ready

  while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET);

  // 4. Set system clock dividers

  RCC_USBCLKConfig(RCC_USBCLKSource_PLLCLK_1Div5);

  RCC_ADCCLKConfig(RCC_PCLK2_Div8);

  RCC_PCLK2Config(RCC_HCLK_Div1);

  RCC_PCLK1Config(RCC_HCLK_Div2);

  RCC_HCLKConfig(RCC_SYSCLK_Div1);

  /*&sharpdefine EMB_FLASH

&sharpifdef EMB_FLASH

  // 5. Init Embedded Flash

  // Zero wait state, if 0 < HCLK 24 MHz

  // One wait state, if 24 MHz < HCLK 56 MHz

  // Two wait states, if 56 MHz < HCLK 72 MHz

  // Flash wait state

  FLASH_SetLatency(FLASH_Latency_2);

  // Half cycle access

  FLASH_HalfCycleAccessCmd(FLASH_HalfCycleAccess_Disable);

  // Prefetch buffer

  FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);

&sharpendif // EMB_FLASH */

 

  // 5. Clock system from PLL

  RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);

---------------------------------------------------------------------------------------------

//Function that manage TIM1

void tim1_init(void){

/*-------TIMER START----------*/

 TIM_TimeBaseInitTypeDef TIM1_TimeBaseInitStruct;

  // Timer1 Init

  // Enable Timer1 clock and release reset

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1,ENABLE);

  RCC_APB2PeriphResetCmd(RCC_APB2Periph_TIM1,DISABLE);

  /*-----------------SETTAGGIO PARAMETRI TIMER1----------------*/

  //  Prescaler=7200  &   Period=10000 & Repetition =0-->Trigger event ogni secondo

  //  Prescaler=3600  &   Period=10000 & Repetition =0-->Trigger event ogni 0.5 secondi

  //  Prescaler=720   &   Period=10000 & Repetition =0-->Trigger event ogni 100ms

  //  Prescaler=6534  &   Period=10   & Repetition =0-->Trigger event ogni 1ms

  /*-----------------------------------------------------------*/

  TIM1_TimeBaseInitStruct.TIM_Prescaler = 1; 

  TIM1_TimeBaseInitStruct.TIM_CounterMode = TIM_CounterMode_Up;

  TIM1_TimeBaseInitStruct.TIM_Period = 1; 

  TIM1_TimeBaseInitStruct.TIM_ClockDivision = TIM_CKD_DIV1;

  TIM1_TimeBaseInitStruct.TIM_RepetitionCounter = 0;

  TIM_TimeBaseInit(TIM1,&TIM1_TimeBaseInitStruct);

  // Clear update interrupt bit

  TIM_ClearITPendingBit(TIM1,TIM_IT_Update);

  // Enable update interrupt

  TIM_ITConfig(TIM1,TIM_IT_Update,ENABLE);

  NVIC_InitTypeDef NVIC_InitStructure; //create NVIC structure

  NVIC_InitStructure.NVIC_IRQChannel = TIM1_UP_TIM16_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

  // Enable timer counting

  TIM_Cmd(TIM1,ENABLE);

/*---------END TIMER----------*/ 

}

void TIM1_UP_TIM16_IRQHandler(void){

...

}

#problem #tim1 #stm32 #timer #interrupt
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on November 05, 2015 at 21:18

Update is the reset/zero event, ie rolls to zero, you yes you'll get that initial interrupt. You'll have to manage that if it's critical to your process. ie use a flag, and ignore the first entry.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..