cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F100 enter standby mode

Posted on August 17, 2010 at 10:41

STM32F100 enter standby mode

3 REPLIES 3
Posted on May 17, 2011 at 14:02

Hi,

Could you please try our example

''STM32F10x_StdPeriph_Lib_V3.3.0\Project\STM32F10x_StdPeriph_Examples\PWR\STANDBY''  and let me know if you observe the same behavior.

Cheers,

STOne-32

gil2
Associate II
Posted on May 17, 2011 at 14:02

I've tried that example and currently do it like this:

...

   // Peripheral Clock - This is done in the init function, but I did it again here

   RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR,ENABLE);

  

   // Enable WKUP pin

   PWR_WakeUpPinCmd(ENABLE);

   // Insert a delay  - I have also tried without this delay

   Delay(0xFFFF);   // for(; nCount != 0; nCount--);

   // Request to enter STANDBY mode and wake up with rising edge of WKUP pin  

   PWR_EnterSTANDBYMode();

   while(1)  

   {  

     // Infinite loop - It's OK because the system will reset anyways  

   }  

The unit does not wake up (reset).  I've tried with both the JTAG connected and not connected.

Port PA.0 (WKUP pin) has a pull-down resistor, leading to a momentary switch, with Vcc on the other side of the switch, which should be enought to generate the required rising edge when the button is pressed.

Thanks!

Posted on May 17, 2011 at 14:02

I found the problem in my code: forgot to enable the peripheral clock for the power control periphery.

now it works!