2010-08-17 1:41 AM
STM32F100 enter standby mode
2011-05-17 5:02 AM
Hi,
Could you please try our example ''STM32F10x_StdPeriph_Lib_V3.3.0\Project\STM32F10x_StdPeriph_Examples\PWR\STANDBY'' and let me know if you observe the same behavior. Cheers, STOne-322011-05-17 5:02 AM
I've tried that example and currently do it like this:
...// Peripheral Clock - This is done in the init function, but I did it again here
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR,ENABLE); // Enable WKUP pin PWR_WakeUpPinCmd(ENABLE);// Insert a delay - I have also tried without this delay
Delay(0xFFFF); // for(; nCount != 0; nCount--);// Request to enter STANDBY mode and wake up with rising edge of WKUP pin
PWR_EnterSTANDBYMode();while(1)
{ // Infinite loop - It's OK because the system will reset anyways } The unit does not wake up (reset). I've tried with both the JTAG connected and not connected. Port PA.0 (WKUP pin) has a pull-down resistor, leading to a momentary switch, with Vcc on the other side of the switch, which should be enought to generate the required rising edge when the button is pressed. Thanks!2011-05-17 5:02 AM
I found the problem in my code: forgot to enable the peripheral clock for the power control periphery.
now it works!