2016-01-14 6:48 AM
2016-01-15 3:14 AM
Hi jeremy_cis,
Can you provide further information about : - Source of system reset: resume from standby/ PVD/ BOR... ? - The main function; how you are managing resuming from system reset / calling RTC Init/Config functions. -Hannibal-2016-01-18 7:39 AM
Hi Hannibal,
The source of system reset is the NRST pin of the microcontroller. I'm currently testing putting that pin down manually, but the debugger ST-LINK / V2 ISOL also causes the microcontroller reset by software when running in debug mode. This causes the same problem. I don't managing resuming from system reset. As an example follows a main.c archive that is with this problem. If the string ''str'' is read can be seen the value of date and time and below I call the function that modifies these values. If you connect the microcontroller without performing a reset, you can see the value being reconfigured every time, but if a reset is performed, AT_RTC function will have no effect on the values. ________________ Attachments : main.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0tJ&d=%2Fa%2F0X0000000bfC%2F7SeKdlKsT9n9UbxKT1c_LtQMSYYspHOiMgOcvO9Z4gg&asPdf=false2016-03-31 6:16 AM
Hi Freya,
It seems that your problem is coming from a bad switching between Power-ON and resuming from Standby/RESET states like this [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F437%20exiting%20standby%20incorrectly¤tviews=63]request.Take a look to my recommendation there.-Hannibal-