2020-12-07 12:11 AM
I am trying to test the CAN bus on STM32F042K6 Nucleo board. I can transmit data but cannot receive. Here is my settings. Data is sent from STM32H7 -Disco board whose CAN0 bitrate is set to 250K. I can send and receive data to/from STM32H7 board. So I know STM32H7 works. But STM32F042K6 Nucleo can transmit to STM32H7 but cannot receive the data. STM32H7 board has embedded transceiver, and STM32F042 I have an external CAN Waveshare transceiver. I confirm the data on both ends using logic analyzer.
On STM32F042K6-Nucleo, the can settings are:
Prescalar: 4
Time Quantum: 500ns
Tq BS1: 4
Tq BS2: 3
SJW: 1
Operating mode: normal
Pin PA11 (D10 on Nucleo Header): CAN_RX
Pin PA12 (D2 on Nucleo Header): CAN_TX
With these settings, Transmit works with 250Kb which I confirmed with logic analyzer and on STM32H7 board receive.
On the STM32F042 RX line, I also confirmed data comes in to pin PA11 with same bitrate (4us for a bit) periodically using logic analyzer.
Here's the code which I am polling. GetRx call always end up in HAL_Error with error parameter 0x200000.
What am I doing wrong ? I appreciate if anyone can help. I am new to CAN protocol.
Thanks
MX_CAN_Init();
/* USER CODE BEGIN 2 */
HAL_StatusTypeDef status;
HAL_StatusTypeDef txstatus;
HAL_StatusTypeDef rxstatus;
if (HAL_CAN_Start(&hcan) == HAL_OK) {
status = HAL_UART_Transmit(&huart2, "CAN Start OK\r\n", 14, HAL_MAX_DELAY);
}
uint8_t txData[8] = { 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08} ;
CAN_TxHeaderTypeDef txHeader;
txHeader.StdId = 0x123;
txHeader.RTR = CAN_RTR_DATA;
txHeader.IDE = CAN_ID_STD;
txHeader.DLC = 8;
uint32_t txMailBox;
CAN_RxHeaderTypeDef rxHeader;
rxHeader.IDE = CAN_ID_STD;
rxHeader.DLC = 8;
rxHeader.StdId = 0x123;
rxHeader.RTR = CAN_RTR_DATA;
uint8_t rxData[8] = {0};
for(int ii=0;ii<8;++ii) rxData[ii] = 0;
char uartBuffer[100];
volatile uint32_t err = 0;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_Delay(1000);
// txstatus = HAL_CAN_AddTxMessage(&hcan, &txHeader, txData, &txMailBox);
// if (txstatus == HAL_OK) {
// status = HAL_UART_Transmit(&huart2, "CAN Transmit OK\r\n", 17, HAL_MAX_DELAY);
// }
uint32_t rxlevel0 = HAL_CAN_GetRxFifoFillLevel(&hcan, CAN_RX_FIFO0);
uint32_t rxlevel1 = HAL_CAN_GetRxFifoFillLevel(&hcan, CAN_RX_FIFO1);
sprintf(uartBuffer, "RxFifoLevel:%u,%u\r\n", rxlevel0,rxlevel1);
status = HAL_UART_Transmit(&huart2, uartBuffer, 20, HAL_MAX_DELAY);
rxstatus = HAL_CAN_GetRxMessage(&hcan, CAN_RX_FIFO0, &rxHeader, rxData);
if (rxstatus == HAL_OK) {
status = HAL_UART_Transmit(&huart2, "CAN Receive OK\r\n", 16, HAL_MAX_DELAY);
}
err = HAL_CAN_GetError(&hcan);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
Solved! Go to Solution.
2020-12-07 12:38 AM
I don't think this code would work for me and I have specifically seen the same problem on my STM32F4 series. For me it was not setting up the HW filters on this device.
I can't give you the complete code for it because mine is a little mashed between other things. But it ends in this: HAL_CAN_ConfigFilter
Try setting up something in CAN_FILTERMODE_IDMASK and setting both FilterMaskIdLow and FilterMaskIdHigh to 0x0000
That should get you listening to everything.
2020-12-07 12:38 AM
I don't think this code would work for me and I have specifically seen the same problem on my STM32F4 series. For me it was not setting up the HW filters on this device.
I can't give you the complete code for it because mine is a little mashed between other things. But it ends in this: HAL_CAN_ConfigFilter
Try setting up something in CAN_FILTERMODE_IDMASK and setting both FilterMaskIdLow and FilterMaskIdHigh to 0x0000
That should get you listening to everything.
2020-12-07 6:50 AM
I put my settings here now
2020-12-07 9:50 AM
Hello David,
Thank you so much. It worked finally. My filter config was not good.