2015-09-30 07:59 AM
Hello,
i use STM32F042C6 MCU and change SYSCFG MEM_MODE to 1 (System Flash memory mapped at 0x00000000) but always see Main Flash (0x08000000) data from address 0x00000000.Also i try set 11 (Embedded SRAM mapped at 0x00000000) but unsuccess.Also i try jump to system bootloader (0x1FFFC400) but MCU back to 0x08000000 vector after small delay (with USB connected).Can anybody use software jump to system bootloader ? #stm32f02015-09-30 08:25 AM
Hi Mitek,
It seems that you haven't update the BOOT0 pin (it has to be set to 1).Did you tried using the ST-Link Utility?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.