STM32F04 CAN RX Interrupt hits twice then stops
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-13 12:53 AM
I migrated the HAL libraries to the latest one. I had been working on my CAN TX Queue but not it looks like my CAN1_RX0_IRQHandler is called twice. The first one gets a good CAN packet, the second time looks like it detects an error and then it never gets called again.
During my migration to the new HAL library, I need to made this change to my code:
void HAL_CAN_RxCpltCallback(CAN_HandleTypeDef* CanHandle)
{ if(CanHandle == NULL) return; CCanBus *pCanBus = (CCanBus*) CanHandle->pObject; // call the aplication callback function if (pCanBus->canEventCallback != NULL) pCanBus->canEventCallback(pCanBus->pCallbackObject, Callback_RX);if (CanHandle->State == HAL_CAN_STATE_BUSY_TX)
// CanHandle->State = HAL_CAN_STATE_BUSY_TX_RX; CanHandle->State = HAL_CAN_STATE_BUSY_TX_RX0; else { //CanHandle->State = HAL_CAN_STATE_BUSY_RX; CanHandle->State = HAL_CAN_STATE_BUSY_RX0;/* Set CAN error code to none */
CanHandle->ErrorCode = HAL_CAN_ERROR_NONE;/* Enable Error warning Interrupt */
__HAL_CAN_ENABLE_IT(CanHandle, CAN_IT_EWG);/* Enable Error passive Interrupt */
__HAL_CAN_ENABLE_IT(CanHandle, CAN_IT_EPV);/* Enable Bus-off Interrupt */
__HAL_CAN_ENABLE_IT(CanHandle, CAN_IT_BOF);/* Enable Last error code Interrupt */
__HAL_CAN_ENABLE_IT(CanHandle, CAN_IT_LEC);/* Enable Error Interrupt */
__HAL_CAN_ENABLE_IT(CanHandle, CAN_IT_ERR); }if(pCanBus->fifoNumber == 0)
// Enable FIFO 0 message pending Interrupt __HAL_CAN_ENABLE_IT(CanHandle, CAN_IT_FMP0); else // Enable FIFO 1 message pending Interrupt __HAL_CAN_ENABLE_IT(CanHandle, CAN_IT_FMP1); }Where I replaced:// CanHandle->State = HAL_CAN_STATE_BUSY_TX_RX; by
CanHandle->State = HAL_CAN_STATE_BUSY_TX_RX0;So when the CAN1_RX0_IRQHandler gets called for the first time there is a FIFO overrun flag which it is clear by the HAL library and I am able to process a received CAN message.
In the Second time, my callback for CAN error is get called but I am reading the error only. Should I do something else?
Which I dont understand is why the Interrupt stops get called? does the HAL library somehow disabling it?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-13 1:06 AM
Some extra info I found.
When entering to the RX interrupt for the first time and the following function is returning a value of 3
__HAL_CAN_MSG_PENDING -> 3
Which means I have 3 pending CAN messages, the callback is only digesting only 1 CAN message, how can I handle/process the extra 2 messages, the next interrupt will generate an error.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-13 1:31 AM
After digging a little more, on the second interrupt: from the HAL library
tmp1 = __HAL_CAN_MSG_PENDING(hcan, CAN_FIFO0);
tmp2 = __HAL_CAN_GET_IT_SOURCE(hcan, CAN_IT_FMP0); /* Check End of reception flag for FIFO0 */ if((tmp1 != 0U) && tmp2) { /* Call receive function */ CAN_Receive_IT(hcan, CAN_FIFO0); }tmp1 = 2
tmp2 = 0
So I have 2 pending CAN messages but the HAL_CAN_GET_IT_SOURCE returns 0 because a CAN error is detected.
So what is the proper procedure to clear CAN Errors?