cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F030R8T6 Programming Via UART

BG1
Senior
Posted on December 26, 2017 at 16:13

Hello everyone .. 

I have an important question .. 

I am designing a circuit with this MCU and I want it to be programmed via UART lines .. So for this , as far as I read the reference manual , I need to put it to the system memory mode .. Please correct me If I'm wrong , I think all I need to program it via UART as a list is  ;

1. A jumper that draws BOOT0 pin to VDD level ...

2. A button that resets the NRST pin for communicating with Flash Loader Demonstrator Software of ST

3. UART lines ...

4. And of course a proper supply for the MCU (All VDDs and GNDs ..)

When I run the 

Flash Loader Demonstrator 

Software and click next all these are going to be sufficient to advance to the programming page ? What confuses me is the nBOOT1 bit of option register ... Is it automatically change to 1 ?

Thanks in advance ..

#stm32f030r8 #uart #via #flash #program
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0