2014-05-01 09:51 PM
2014-05-02 08:14 AM
Where on earth are you getting these pin designations. Don't confuse the pins on the STM32F103 implementing the ST-LINK/V2 with the pins on the F030 you need to connect to a header.
The STM32F030 is going to use SWD via PA13 SWDIO (JTMS), PA14 SWCLK (JTCK), and NRSThttp://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00088500.pdf
2014-05-04 09:40 PM
thanks sir for reply,
You are right sir, but if i have to make JTAG connection not SWD then may you help me for correct connections2014-05-05 02:08 AM
As best I can tell the part does NOT support JTAG
The wouldn't preclude the use of the 20-pin 0.1'' header, and you could use a JTAG pod supporting Cortex-M0 and SWD