STM32F0 UART not sending data
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-20 2:20 AM
I'm new in ST world. I'm trying to work with UART, so I wrote this code to initializate UART and to send ''Hello''. I'am using STM32F0 board.
#include ''stm32f0xx_gpio.h''
#include ''stm32f0xx_rcc.h''
#include ''stm32f0xx_misc.h''
#include ''stm32f0xx_usart.h''
#define UINT8 uint8_t
#define UINT32 uint32_t
#define MAX_BUFFER_SIZE 256
typedef struct Buffer_st
{
UINT8 size;
UINT8 data[MAX_BUFFER_SIZE];
}Buffer_st;
Buffer_st receivedDataUART1;
void initUART1(UINT32 baudRate)
{
NVIC_InitTypeDef NVIC_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
/* Enable the USART1 Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
//UART init
USART_InitStructure.USART_BaudRate = baudRate;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
/* Enable GPIO clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
/* Enable USART clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
/* Connect PXx to USARTx_Tx */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1);
/* Connect PXx to USARTx_Rx */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1);
/* Configure USART Tx, Rx as alternate function push-pull */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* USART configuration */
USART_Init(USART1, &USART_InitStructure);
/* Enable USART */
USART_Cmd(USART1, ENABLE);
USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);
resetReceivedDataBufferUART1();
}
void resetReceivedDataBufferUART1(void)
{
receivedDataUART1.size = 0;
memset(receivedDataUART1.data, MAX_BUFFER_SIZE, 0);
}
UINT8 sendDataUART1(Buffer_st buffer)
{
UINT8 cpt;
for (cpt = 0; cpt < buffer.size; cpt++)
{
USART_SendData(USART1, buffer.data[cpt]);
//Loop until the end of transmission
while (USART_GetFlagStatus(USART1, USART_IT_TXE) == RESET);
}
}
void USART1_IRQHandler(void)
{
if (USART_GetITStatus(USART1, USART_IT_RXNE) != RESET)
{
receivedDataUART1.data[receivedDataUART1.size++] = USART_ReceiveData(USART1);
}
}
int main(void)
{
Buffer_st buffer = {6,''Hello''};
initUART1(9600);
sendDataUART1(buffer);
while(1);
return 0;
}
I'am using UART/USB connector. The problem is that I don't receive any thing in minicom. When debugging I found that progrom enter in infinite loop
//Loop until the end of transmission while (USART_GetFlagStatus(USART1, USART_IT_TXE) == RESET);
#usart #uart #stm32 #stm32f0 #discovery
- Labels:
-
STM32F0 Series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-20 3:06 AM
Hi
''I'am using STM32F0 board.'' ''I'am using UART/USB connector.'' Are you using this board : If so - stop IMMEDIATELY. You are putting RS232 voltages (+/-12V) into an IO pint that is only 3.3V (5V if it is a 5V tolerant IO) pin! You MUST add a RS232 level converter, such as a MAX232. I do not know if that is the reason for your lock up.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-20 3:22 AM
Yes I'am using STM32F0 discovery board.
Also, I'am using RS232 to 3.3v TTL adapter- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-20 10:06 AM
Simplify, generate a stream of characters, examine the signals with a scope, confirm the nature and speed, and sense of rx/tx with respect to the receiving device.
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
‎2014-10-22 12:09 PM
Finally I resolved the problem.
I was mixing up interrupt status flags with the flags used for synchronous polling. To send data we must first poll the
USART_FLAG_TXE
flag for the
transmit data register emptystatus and then we can send bytes. The
USART_IT_TXE
flag is for interrupt use only.
So the correction is//Loop until the end of transmission
while(USART_GetFlagStatus(USART1,USART_FLAG_TXE)!=SET);
USART_SendData(USART1, buffer.data[cpt]);