cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0 - power

nick239955
Associate II
Posted on October 07, 2012 at 16:57

So I managed to get my boards programmed and working... except one little detail - power consumption is rather high for my application. With both UARTs on and nothing else, running on HSI at 48Mhz, current consumption is at 10.2mA when starting up and 9.5-9.3 once everything is initialized.

Any suggestions towards lowering that? Ideally under 5mA... if that's even possible?

Would hate having to switch to STM32L* now that all code was done? 

TIA!
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
frankmeyer9
Associate II
Posted on October 10, 2012 at 12:34

You may be right, the cpu core uses all four cycles to process single instruction, really simple cpu.

 

I understand ''really simple cpu'' as euphemism for ''botched''.

I have to work with this thing, which is not really funny...