2013-08-30 12:33 AM
Hi,
finally it was decided to work with the micro stm32F0 and Keil's products. If I wanted to load my program without ULink device but through rs-232, can I do it? Is there a guide ? I know that there is STMFlashLoader, but I don't know whether it's suitable for micro STM32F0. If I can use STMFlashLoader, which file do I have to load (.axf or .hex )? THANKS2013-09-23 07:01 AM
Hi Simone,
The version 2.6.0 of the FlashLoader supports STM32F0xx devices. You can download it from thishttp://www.st.com/web/en/catalog/tools/PF257525
. The UM0462 on same page should be helpful besides to . -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.