2013-03-21 2:46 AM
Hi,
64 byte transfers from my STM32F4 cdc driver to the host side fails. 63 bytes work, as well as 65 bytes. A quick forum search indicates that this is a bug in the cdc class driver firmware. A 64 byte transfer should be followed by a 0-byte transfer so that the host side (windows) can detect end of transfer. So, this bug is known but I have so far failed to find a fix for it. Does anyone know how to fix it - or is there a firmware library out there somewhere where this is fixed already? Currently I'm using ''STM32_USB-Host-Device_Lib_V2.1.0'', V1.1.0 / 19-March-2012 Best regards, Mikael2013-03-22 2:04 AM
Hi Mikael,
I am working with USB VCP example recently. I am not sure whether following modification could fix the bug. /** * @brief Handle_USBAsynchXfer * Send data to USB * @param pdev: instance * @retval None */ static void Handle_USBAsynchXfer (void *pdev) { uint16_t USB_Tx_ptr; static uint16_t USB_Tx_length = 0; if(USB_Tx_State != 1) { if (APP_Rx_ptr_out == APP_RX_DATA_SIZE) { APP_Rx_ptr_out = 0; } if(APP_Rx_ptr_out == APP_Rx_ptr_in) { if(USB_Tx_length == CDC_DATA_MAX_PACKET_SIZE) { USB_Tx_length = 0; } else { USB_Tx_length = 0; USB_Tx_State = 0; return; } } else if(APP_Rx_ptr_out > APP_Rx_ptr_in) /* rollback */ { APP_Rx_length = APP_RX_DATA_SIZE - APP_Rx_ptr_out; } else { APP_Rx_length = APP_Rx_ptr_in - APP_Rx_ptr_out; } #ifdef USB_OTG_HS_INTERNAL_DMA_ENABLED APP_Rx_length &= ~0x03; #endif /* USB_OTG_HS_INTERNAL_DMA_ENABLED */ if (APP_Rx_length > CDC_DATA_IN_PACKET_SIZE) { USB_Tx_ptr = APP_Rx_ptr_out; USB_Tx_length = CDC_DATA_IN_PACKET_SIZE; APP_Rx_ptr_out += CDC_DATA_IN_PACKET_SIZE; APP_Rx_length -= CDC_DATA_IN_PACKET_SIZE; } else { USB_Tx_ptr = APP_Rx_ptr_out; USB_Tx_length = APP_Rx_length; APP_Rx_ptr_out += APP_Rx_length; APP_Rx_length = 0; } USB_Tx_State = 1; DCD_EP_Tx (pdev, CDC_IN_EP, (uint8_t*)&APP_Rx_Buffer[USB_Tx_ptr], USB_Tx_length); } } Best regards, Tyrone2013-03-22 2:58 AM
Sorry,
usbd_cdc_DataIn() also calls DCD_EP_Tx(CDC_IN_EP), then static uint16_t USB_Tx_length = 0 should be seen in the whole file. Best regards, Tyrone