STM32CubeProgrammer "Warning: The core is locked up"
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-27 1:51 PM
Hi,
When programming STM32F303VCT6 chips using STLINK-V3SET programmers via a jtag connection and STM32cubeProgrammer I get "Warning: The core is locked up" and the board doesn't operate normally. Here is the log output:
14:19:12 : UR connection mode is defined with the HWrst reset mode
14:19:12 : ST-LINK SN : 0039001E4D4B500E20373831
14:19:12 : ST-LINK FW : V3J8M3B5S1
14:19:12 : Board : STLINK-V3SET
14:19:12 : Voltage : 3.29V
14:19:12 : SWD freq : 8000 KHz
14:19:12 : Connect mode: Normal
14:19:12 : Reset mode : Software reset
14:19:12 : Device ID : 0x422
14:19:12 : Revision ID : Rev Y
14:19:12 : Debug in Low Power mode is not supported for this device.
14:19:13 : UPLOADING OPTION BYTES DATA ...
14:19:13 : Bank : 0x00
14:19:13 : Address : 0x1ffff800
14:19:13 : Size : 16 Bytes
14:19:13 : UPLOADING ...
14:19:13 : Size : 1024 Bytes
14:19:13 : Address : 0x8000000
14:19:13 : Read progress:
14:19:13 : Data read successfully
14:19:13 : Time elapsed during the read operation is: 00:00:00.003
14:19:30 : Memory Programming ...
14:19:30 : Opening and parsing file: 230209.bin
14:19:30 : File : 230209.bin
14:19:30 : Size : 100.54 KB
14:19:30 : Address : 0x08000000
14:19:30 : Erasing memory corresponding to segment 0:
14:19:30 : Erasing internal memory sectors [0 50]
14:19:31 : Download in Progress:
14:19:35 : File download complete
14:19:35 : Time elapsed during download operation: 00:00:04.741
14:19:35 : Verifying ...
14:19:35 : Read progress:
14:19:35 : Download verified successfully
14:19:35 : RUNNING Program ...
14:19:35 : Address: : 0x08000000
14:19:35 : Warning: The core is locked up
14:19:35 : Start operation achieved successfully
Here's what I've tried so far
- Same thing happens with known good standard versions of this PCB, so not the PCB/MCU
- Updated STM32CubeProgrammer from V2.7.0 to V2.14.0, get the same error
- Swapped out USB cable and ports, nope
- Swapped out PSU to the PCB/MCU and confirmed the supply voltage, no issues here
- Swapped out STLINK to a brand new one, no change
- Restarted PC, Yeah, I did and no change.
What the heck else could the problem be?
Solved! Go to Solution.
- Labels:
-
STM32F3 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-28 7:22 AM
It's working now... I think the issue was the Google Drive desktop shared folder that the firmware file was in. I've had issues with it in the past, so I decided to download the file from the Google Drive web interface to my hard disk this morning and it worked, but now it also works from the Drive desktop folder.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-27 2:03 PM - edited ‎2023-09-27 2:19 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-27 3:47 PM
Hi Issamos,
RDP was already set to 0xAA, but I tried changing it to 0xBB, applying it, and switching back to AA, but no dice. Same issue. Also, I can't find PCROP as mentioned in that post. I could try that if you could point me in the right direction.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-28 6:33 AM
Just a guess but possibly try "Reset mode" set to "Hardware".
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-28 7:22 AM
It's working now... I think the issue was the Google Drive desktop shared folder that the firmware file was in. I've had issues with it in the past, so I decided to download the file from the Google Drive web interface to my hard disk this morning and it worked, but now it also works from the Drive desktop folder.