2016-09-02 4:38 AM
Hi,
is there the possibility to change the ''Vdd Power Supply'' values inside of the Parameter Selection. I would like to select 2.8V but doesn't have the possibility to do so. Also small file hacks are welcome...Thanks in advance.2016-09-02 8:08 AM
Hi banjoBazooka,
The power consumption calculator (PCC) in STM32CubeMX returns Average of current consumption, Battery life… these data are taken from the MCU datasheet or interpolated from a user specified bus or core frequency.VDD parameter is fixed according to VDD values presented on datasheets.Otherwise I will raise this request to our MX team as enhancement.-Syrine-2016-09-05 12:53 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.