Skip to main content
Phillip Wolstencroft
Associate II
May 17, 2017
Question

STM32CubeMX plugin crashes in Truestudio requiring TrueSTUDIO restart

  • May 17, 2017
  • 2 replies
  • 1820 views
Posted on May 17, 2017 at 08:26

Using W7 with latest version of TrueSTUDIO V7.1.2.

Latest version of STM32CubeMX V4.21.0 eclipse plugin.

Start project in STM32CubeMX for Nucleo-F030R8 or Nucleo-F072RB and start defining setup.

CubeMX often requests to save project which after approx 2 saves it locks up. TrueSTUDIO still works but you have to restart TrueSTUDIO to get CubeMX working again.

    This topic has been closed for replies.

    2 replies

    Nesrine M_O
    Associate
    May 17, 2017
    Posted on May 17, 2017 at 10:46

    Hi

    Wolstencroft.Phillip

    ,

    I'll report this issue to our MX team for checking;Sorry for the inconvenience it may bring.

    -Nesrine-

    Jeanne Joly
    Associate
    January 16, 2018
    Posted on January 16, 2018 at 16:16

    Hi,

    Sorry for the late answer.

    When you say ' Start project in STM32CubeMX for Nucleo-F030R8 or Nucleo-F072RB and start defining setup.

    CubeMX often requests to save project which after approx 2 saves it locks up. TrueSTUDIO still works but you have to restart TrueSTUDIO to get CubeMX working again.'

    What do you mean by defining setup (which steps?)?

    I load the Nucleo board F030R8 and generate project with TrueStudio with CubeMX4.23. I don't have to restart TrueSTUDIO to get CubeMX working again.

    Please, sens us your ioc file if the problem persists and give us more details in order to help you.

    BR. Jeanne

    Phillip Wolstencroft
    Associate II
    January 16, 2018
    Posted on January 16, 2018 at 21:50

    Hi Jeanne,

    Sorry, it has been so long since I played with TrueStudio I can't fully

    remember the exact scenario. I have since purchased Sommnium, just

    before they ceased trading, am currently using Keil free version for F0

    series.

    If I can interpret my words concerning 'defining setup' correctly, I

    assume I was referring to the process of peripheral and I/O setup.

    I only ever had the problem with the plug in into Truestudio, never with

    the stand-alone cubeMX.

    In my recollections, I think when you would go in to edit the settings

    the system would require you to do a save and often when you did this it

    would lock up. Sorry I can't be more informative but I just can't

    remember fully the complete scenario.

    A question for you. I assume this inquiry is in preparation for your

    release of the new Truestudio free release for ST customers. Can you

    tell me if Keil's RTX OS is able to be supported under Truestudio? I

    always liked Truestudio but they did the dirty (I believe IMHO) on their

    customers with big price hikes and, how I saw it, misleading them with

    their initial reasonable monthly subscription to way overpriced. I would

    like to use Truestudio again but am now sort of locked in with RTX code.

    regards

    Phil

    Jeanne Joly
    Associate
    January 17, 2018
    Posted on January 17, 2018 at 16:10

    Hi

    Wolstencroft.Phillip

    ,

    Regarding your question 'Can youtell me if Keil's RTX OS is able to be supported under Truestudio?', Truestudio pro will be soon available and free only for STM32 (which supports FreeRTOS).

    Truestudio Lite supports STM32 (FreeRTOS).

    BR. Jeanne