cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX PCC tool

kswST
Associate II

I’m trying to understand the peripheral current consumption figures generated by the PCC tool in CubeMX for my STM32U031 based project but can’t correlate the generated numbers with the values given in Table 43 of the datasheet, so I’m wondering which is likely to be correct, the PCC values or datasheet values?

I’m also struggling to understand what the names used in the PCC ‘Peripheral Selection’ tab tick-boxes refer to; e.g. TIM1 vs TIM1/SYS, PWR/TIM2,  ADC1/SYS vs ADC1 CLK_KER_SYS etc etc, as there’s no help in the tool, or guidance in the UM1718, so any help here would be much appreciated!

0 REPLIES 0