2017-02-09 11:12 AM
Hello all,
I am using STM32CubeMX Version 4.19.0. I developed my project using Nucleo F446ZE which uses the LQFP package. It's all working great so now I need to move to the deployed package which is the F446ZEH UFBGA. Here is what I did in Cube:
ADC_CHANNEL_TEMPSENSOR and they are identical.
So I can't be sure, but I'm more inclined to think this warning from Cube is bogus. Any confirmation of that, either way, would be appreciated.
Thanks for reading.
2017-02-13 1:41 AM
Hi
Downey.Elwood
,Please follow steps in the
/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Fuser_manual%2F10%2Fc5%2F1a%2F43%2F3a%2F70%2F43%2F7d%2FDM001047pdf%2Ffiles%2FDM001047pdf%2Fjcr%3Acontent%2Ftranslations%2Fen.DM001047pdf
,Tutorial 5:exporting current project configuration to a compatible MCU
,then tell us about the result.-Nesrine-