2015-07-14 01:18 AM
I have installed STM32CUBEMX 4.9.0. on my Win7 PC. Using Help/Install New Libraries I can download and install for example Firmware Package for Family STM32F4. However, Help/Check for Updates (or the Check button in the New Libraries Manager pane) produces an error with the Connection to HTTP Server green progress bar stopped at about 50% and the pop up message ''Error during Access to HTTP Server. Please check Proxy ...''
I am using the Use System Proxy Parameters setting but have also tried a manual configuration that works OK with Rowley CrossWorks IDE. Pressing the Check connection button always brings up a green tick regardless of the Proxy Server Type radio button setting. Is this a CubeMX problem? Any advice please?2015-07-14 03:03 AM
Hi John,
I have installed the cubeMx 4.9.0 and I have updated many packages with no problem. Do you use credential sharing? I suspect that the problem is related to your proxy settings. Best regards2015-07-14 03:21 AM
Hi thanks for your response. I work in a secure commercial environment so it's likely the problem is at our end. I just wanted to enquire here first before getting our IT department involved. As I said, the file download works fine but the update check doesn't. I wondered why one part worked when the other doesn't.
2015-07-15 07:54 AM
Hello John,
Your issue has not been reproduced. Do you still encounter the error? Thanks for your feedback.2015-07-15 08:22 AM
Hi,
Thanks for following this up. Today - it works. I am using the Use System Proxy Parameters setting and have made no changes. The PC has been powered down overnight and up again this morning. I can't explain it but for now anyway both ''Check for Updates'' and ''Install New Libraries'' are working!2015-07-17 06:00 AM
Good news.
Thank you John for the feedback.