cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 4.14.0 fails to install on Ubuntu 16.04

rchrdlyon1
Associate II
Posted on May 16, 2016 at 17:52

STM32CubeMX 4.14.0 fails to install on Ubuntu 16.04

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
rchrdlyon1
Associate II
Posted on May 16, 2016 at 18:00

Some details:

Ubuntu 16.04 64-bit Desktop with Oracle Java SE 1.8.0_92 64-bit. Installation always fails with the following output:

> sudo ./SetupSTM32CubeMX-4.14.0.linux

> [sudo] password for rlyon:

sudo: unable to execute ./SetupSTM32CubeMX-4.14.0.linux: No such file or directory

Downloaded archive again and tried to install with same result. Then tried to install previous version 4.13.0 and it works perfectly. Anyone else had this problem with Ubuntu 16.0.4? There must be some installer dependency missing?

Nesrine M_O
Lead II
Posted on May 17, 2016 at 13:05

Hi lyon.richard,

I'll report this issue to our MX team for checking. Sorry for the inconvenience it may bring.

-Syrine –
stm32cube-t
ST Employee
Posted on October 07, 2016 at 18:05

Dear user,

We don't reproduce your issue. Do you still have problems with our latest release 4.16.1?

Best regards

Eldar Qurbanov
Associate
Posted on November 26, 2017 at 19:41

I have the same problem installing CubeMX in ubuntu 16.4

java -version

openjdk version '1.8.0_151'

OpenJDK Runtime Environment (build 1.8.0_151-8u151-b12-0ubuntu0.16.04.2-b12)

OpenJDK 64-Bit Server VM (build 25.151-b12, mixed mode)

./SetupSTM32CubeMX-4.23.0.linux

bash: ./SetupSTM32CubeMX-4.23.0.linux: No such file or directory

sudo java -jar SetupSTM32CubeMX-4.23.0.exe

sudo: unable to resolve host rmzn-linux

Nov 26, 2017 10:36:01 PM INFO: Logging initialized at level 'INFO'

Nov 26, 2017 10:36:01 PM INFO: Commandline arguments:

Nov 26, 2017 10:36:02 PM INFO: Detected platform: ubuntu_linux,version=4.14.2-041402-lowlatency,arch=x64,symbolicName=null,javaVersion=1.8.0_151

Nov 26, 2017 10:36:02 PM WARNING: Failed to determine hostname and IP address

==> worked installed in  /usr/local/STMicroelectronics/STM32Cube/STM32CubeMX/  but cannot run also 

BTW  I installed it ubuntu 14.4 works well