2024-01-11 7:20 AM
After some time I found the tool displaying an error of sort, I think something regarding inactivity.
Following that I can't close the sampling window. I can't move it or minimize it , or press any button in its GUI. All buttons are unresponsive.
I can open a new instance of the STM32CubeMonitor-Power, and I can move to other Windows apps.
But the windows is still there. Stuck.
2024-01-31 7:13 AM
I have the same problem with STLINK-V3PWR.
The data are still writing by address c:\Users\veaceslav\AppData\Local\Temp\Power_Monitor\Acquisition\2024_01_31_15_40_03_2, but apps doesn't response on clics. I can't stop it, and save data.
2024-04-07 10:52 PM
I have the same problem using STLINK-V3PWR and STM32CubeMonPwr V1.21.
It seems to happen after a while with acqusition time set to infinity.