cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeF1 startup file

Jian Chen
Associate II
Posted on January 21, 2017 at 18:40

Hi,

I downloaded stm32cubef1 firmware package.  I am using examples on STM3210E_EVAL projects.  With the EWARM(IAR embedded workbend for ARM), I see all examples use startup_stm32f103xg.s as start up file.

I am using STM32F103RET6 device, not STM32F103ZGT6 used on the STM3210E_EVAL board.   What changes do I need to make to create startup_stm32f103xe.s file?

Thanks, Jian

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nesrine M_O
Lead II
Posted on January 23, 2017 at 14:11

Hi

chen.jian.005

,

To find your appropriate startup file please refer to this path STM32Cube_FW_F1_V1.4.0\Drivers\CMSIS\Device\ST\STM32F1xx\Source\Templates\iar

-Nesrine-

Ifmy suggestanswers your question, please mark it as correct.