STM32CubeF1 Firmware Package V1.8.6 和STM32CubeF1 Firmware Package V1.8.5有什么区别
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-03-21 1:24 AM
本人在实践过程中遇到一个问题。项目中需要用到外置flash芯片-W25q128。本人计划用f103C8T6的SPI2、DMA去通讯。用的是cube生成的工程文档。
第一次用的是STM32CubeF1 固件包 v1.8.6。串口打印不出flash芯片的ID号,串口发送0x0。
花了一天检查,最后用STM32CubeF1 Firmware Package v1.8.5。串口打印成功了,falsh芯片的ID 号为0xEF17.
请问这2个版本的包中对SPI2和DMA有啥异同吗?
Labels:
- Labels:
-
STM32CubeMX
-
STM32F1 Series
0 REPLIES 0