2017-09-13 09:57 PM
Hello!
Basically the title explains all. Here are a few details.
I'm using IAR 8.11, and I'm trying to compile sample code from STM32Cube_FW_F4_V1.16.0, with the board I have: a STM32469I-Disco. I tried to compile all the examples related to LCD, none of them works. I was told it's probably a problem in STM32Cube_FW_F4_V1.16.0 which should be use with IAR 7. I was told that 7.8 works.
Will there be an update to these firmwares (V1.17 for example) anytime soon?
Best regards,
R
2017-09-13 11:01 PM
You might want to ask yourself why 8.x is incompatible with prior releases, and what else in your code base this might affect adversely. Does IAR provide a compatibility mode/setting?