cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cubeâ„¢ extended to support STM32F2 MCUs

Amel NASRI
ST Employee
Posted on April 08, 2014 at 10:15

STMicroelectronics Extends STM32Cube™ Development Platform to Support Market-Proven STM32 F2 Microcontrollers

 

0690X00000605eBQAQ.png

STMicroelectronics has released a further set of middleware for its

STM32Cube™

development platform announced in February, allowing developers to target 

http://www.st.com/web/en/catalog/mmc/FM141/SC1169/SS1575

microcontrollers.

The 

http://www.st.com/web/en/catalog/tools/PF260266

is currently available for the STM32 F2 and F4 series and further releases will roll out during 2014, extending support to all STM32 devices.

Developers can quickly generate initialization code for their applications using The 

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF259242

graphical configuration tool.

For further information and to download STM32Cube free of charge, please visit

http://www.st.com/stm32cube

.

STM32CubeF2

http://www.st.com/web/en/news/n3543

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0