2025-03-04 4:05 AM - last edited on 2025-03-04 4:55 AM by mƎALLEm
Greetings Everybody,
I am trying my hands with CAN FD. I have selected STM32C092RC for the same application as it has can fd port.
I was wondering if MCP2561/62 can fd transiver ic works with this controller. Please advice. I was also looking for schematic and cad resources for NUCLEO-C092RC board, but cant find. If anybody has the link for cad resources and schematics for NUCLEO-C092RC board then please do forward it.
Thanks in advance.
2025-03-04 4:52 AM - edited 2025-03-04 5:18 AM
Hello @Nimit Vachhani ,
1- MCP2561 is OK. But please select the version having VIO pin. But becarefull this transceiver could not exceed 1Mb/s if you are planning to use CAN-FD data rate > 1Mb/s:
If you plan to exceed that bitrate, I may suggest MCP2562FD that can reach up to 8Mb/s.
2- For the schematic and cad resources for NUCLEO-C092RC board, they are not yet available on the ST website.
It will be available soon. For the moment, you can rely on the UM3353.
Edit: NUCLEO-C092RC has already a CAN-FD transceiver:
No need to add another CAN transceiver.
And this is the CAN connector (in green) correspond to CAN_H and CAN_L + GND (I think):
Hope that answers your questions.