2015-02-23 2:53 PM
Hello everyone,
I juste received an ulinkpro so I can use the ETM feature later on in my development. Right now, I am trying to simply display a variable in the logic analyzer but I get no synchronization. I read that we must link a .ini file to configure the board for traces.Anyone has already done it? What should I do.Regards,Keaven #stm324x9i-eval-trace-ulinkpro2015-02-23 3:45 PM
Anyone has already done it? What should I do.
Read the manual(s), talk to Keil support? Have done for the MCBSTM32F400, needed to jumper the high order address pins so they go to the trace header, not the external memories. Create a debugger script (.INI) to bring up the board. So you'd definitely want to read the board manual and know exactly what jumpers or solder bridges need setting.2015-02-23 4:01 PM
C:\Keil470\ARM\Boards\Keil\MCBSTM32F400\Blinky_ULp\STM32F4xx_TP.ini
/******************************************************************************/
/* STM32_TP.ini: STM32 Debugger Initialization File */
/******************************************************************************/
// <<<
Use
Configuration Wizard in Context Menu >>> //
/******************************************************************************/
/* This file is part of the uVision/ARM development tools. */
/* Copyright (c) 2005-2011 Keil Software. All rights reserved. */
/* This software may only be used under the terms of a valid, current, */
/* end user licence from KEIL for a compatible version of KEIL software */
/* development tools. Nothing else gives you the right to use this software. */
/******************************************************************************/
FUNC void DebugSetup (void) {
_WDWORD(0x40023830, _RDWORD(0x40023830) | 0x00000010); // RCC_AHB1ENR: IO port E clock enable
_WDWORD(0x40021000, 0x00002AA0); // GPIOE_MODER: PE2..PE6 = Alternate function mode
_WDWORD(0x40021008, 0x00003FF0); // GPIOE_OSPEEDR: PE2..PE6 = 100 MHz speed
_WDWORD(0x4002100C, 0x00000000); // GPIOE_PUPDR: PE2..PE6 = No Pull-up/Pull-down
_WDWORD(0x40021020, 0x00000000); // GPIOE_AFRL: PE2..PE6 = AF0
// <
h
> Debug MCU Configuration
// <
o1.0
> DBG_SLEEP <
i
> Debug Sleep Mode
// <
o1.1
> DBG_STOP <
i
> Debug Stop Mode
// <
o1.2
> DBG_STANDBY <
i
> Debug Standby Mode
// <
o1.5
> TRACE_IOEN <
i
> Trace I/O Enable
// <
o1.6..7
> TRACE_MODE <
i
> Trace Mode
// <
0
=> Asynchronous
// <
1
=> Synchronous: TRACEDATA Size 1
// <
2
=> Synchronous: TRACEDATA Size 2
// <
3
=> Synchronous: TRACEDATA Size 4
// </
h
>
_WDWORD(0xE0042004, 0x000000E7); // DBGMCU_CR
// <
h
> Debug MCU APB1 Freeze
// <
o1.0
> DBG_TIM2_STOP <
i
> Timer 2 Stopped when Core is halted
// <
o1.1
> DBG_TIM3_STOP <
i
> Timer 3 Stopped when Core is halted
// <
o1.2
> DBG_TIM4_STOP <
i
> Timer 4 Stopped when Core is halted
// <
o1.3
> DBG_TIM5_STOP <
i
> Timer 5 Stopped when Core is halted
// <
o1.4
> DBG_TIM6_STOP <
i
> Timer 6 Stopped when Core is halted
// <
o1.5
> DBG_TIM7_STOP <
i
> Timer 7 Stopped when Core is halted
// <
o1.6
> DBG_TIM12_STOP <
i
> Timer 12 Stopped when Core is halted
// <
o1.7
> DBG_TIM13_STOP <
i
> Timer 13 Stopped when Core is halted
// <
o1.8
> DBG_TIM14_STOP <
i
> Timer 14 Stopped when Core is halted
// <
o1.10
> DBG_RTC_STOP <
i
> RTC Stopped when Core is halted
// <
o1.11
> DBG_WWDG_STOP <
i
> Window Watchdog Stopped when Core is halted
// <
o1.12
> DBG_IWDG_STOP <
i
> Independent Watchdog Stopped when Core is halted
// <
o1.21
> DBG_I2C1_SMBUS_TIMEOUT <
i
> I2C1 SMBUS Timeout Mode Stopped when Core is halted
// <
o1.22
> DBG_I2C2_SMBUS_TIMEOUT <
i
> I2C2 SMBUS Timeout Mode Stopped when Core is halted
// <
o1.23
> DBG_I2C3_SMBUS_TIMEOUT <
i
> I2C3 SMBUS Timeout Mode Stopped when Core is halted
// <
o1.25
> DBG_CAN1_STOP <
i
> CAN1 Stopped when Core is halted
// <
o1.26
> DBG_CAN2_STOP <
i
> CAN2 Stopped when Core is halted
// </
h
>
_WDWORD(0xE0042008, 0x00000000); // DBGMCU_APB1_FZ
// <
h
> Debug MCU APB2 Freeze
// <
o1.0
> DBG_TIM1_STOP <
i
> Timer 1 Stopped when Core is halted
// <
o1.1
> DBG_TIM8_STOP <
i
> Timer 8 Stopped when Core is halted
// <
o1.16
> DBG_TIM9_STOP <
i
> Timer 9 Stopped when Core is halted
// <
o1.17
> DBG_TIM10_STOP <
i
> Timer 10 Stopped when Core is halted
// <
o1.18
> DBG_TIM11_STOP <
i
> Timer 11 Stopped when Core is halted
// </
h
>
_WDWORD(0xE004200C, 0x00000000); // DBGMCU_APB2_FZ
}
// Executed after reset via uVision's 'Reset'-button
FUNC void OnResetExec (void) {
DebugSetup();
}
DebugSetup(); // Debugger Setup
2015-02-24 6:53 AM
Thank you Clive1,
I found some example of debug file for STM32437I-Eval which has the same MCU and looks close to what I have . I will look into it.Will contact Keil for other side of the problem.Thank you