cancel
Showing results for 
Search instead for 
Did you mean: 

stm32439i-eval2 LCD usable definition ?

gilberce
Associate II
Posted on September 11, 2014 at 16:38

Hi,

I was wondering why in the stm32439i-eval2 dev board, the

am640480G5TNQW  LCD is configured to be used in a 480x272 (unusual) defnition.

Is it possible to use it at 640x480 as part of driver allow it ?

Moreover, the camera embedded is a 2MP, so again why the image in the demo is cropped to the lcd definition ?

Regards

#stm32439i-eval2-am640480g5tnqw
2 REPLIES 2
Posted on September 11, 2014 at 17:03

Probably because most of the original STM324x9I-EVAL boards had an MB1046 panel a 16:9 480x272 display? And not the MB1063

I've seen demo packages built for both different panels, inquire via you ST FAE or rep.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
gilberce
Associate II
Posted on September 16, 2014 at 15:35

ty Clive,

I got the 1063, looking for enabling a wider display.

Btw the CAMERA to USB disk is not functionnal on the 1063. The dislay his cut on the bottom half and there are 4 minidisplay with lacking lines on the top.

When I got time I'll look further.

Regards.