STM3210VE, 8G SD card , SDIO 4bits bus, DMA mode-STOne-32,help me please
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2010-09-16 6:07 PM
STM3210VE, 8G SD card , SDIO 4bits bus, DMA mode-STOne-32,help me please
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2011-05-17 5:07 AM
Is R/W SDHC card by SDIO in DMA 4bits mode not s
table
? Are you sure the high capacity cards use the same protocol as the older/slower cards? I'm pretty these cards won't work in classic readers either.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2011-05-17 5:07 AM
thanks for your reply,
This code can judge the type of cards...and i readed the spec: Part_1_Physical_Layer_Simplified_Specification_Ver3.01_Final_100518.pdf and SD_SDIO_specsv1.pdfThe Process
of the code is right for the spec.. And all of the Response for the CMD is right.../* CMD8: SEND_IF_COND --------------------------------------------------------*/
/* Send CMD8 to verify SD card interface operating condition */ /* Argument: - [31:12]: Reserved (shall be set to '0') - [11:8]: Supply Voltage (VHS) 0x1 (Range: 2.7-3.6 V) - [7:0]: Check Pattern (recommended 0xAA) */ /* CMD Response: R7 */ SDIO_CmdInitStructure.SDIO_Argument = SD_CHECK_PATTERN; SDIO_CmdInitStructure.SDIO_CmdIndex = SDIO_SEND_IF_COND; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure);errorstatus = CmdResp7Error();
if (errorstatus == SD_OK)
{ CardType = SDIO_STD_CAPACITY_SD_CARD_V2_0; /* SD Card 2.0 */ SDType = SD_HIGH_CAPACITY; } else { /* CMD55 */ SDIO_CmdInitStructure.SDIO_Argument = 0x00; SDIO_CmdInitStructure.SDIO_CmdIndex = SDIO_APP_CMD; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure); errorstatus = CmdResp1Error(SDIO_APP_CMD); }- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2011-05-17 5:07 AM
I am crazy.who can tell me some c
lue
?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2011-05-17 5:07 AM
越�?�越晕乎了。。。真是的,这问题�?�的,SANDISK的8G SDHC�?�,�?�尔能写,但是文件里�?�大部分的数�?�都是错的。。晕。。。2G的完全正确
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2011-05-17 5:07 AM
Dear lin,
I will be back to you soon, i need to investigate the case and reproduce it first. Cheers, STOne-32.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2011-05-17 5:07 AM
//Now i describe my code to you,and i think there are some bugs in the
//examples which come from st. SD_Error SD_PowerON(void) { SD_Error errorstatus = SD_OK; uint32_t response = 0, count = 0; bool validvoltage = FALSE; uint32_t SDType = SD_STD_CAPACITY; uint8_t i = 0;/* Power ON Sequence -------------------------------------------------------*/
/* Configure the SDIO peripheral */ SDIO_InitStructure.SDIO_ClockDiv = SDIO_INIT_CLK_DIV; /* HCLK = 72MHz, SDIOCLK = 72MHz, SDIO_CK = HCLK/(178 + 2) = 400 KHz */ SDIO_InitStructure.SDIO_ClockEdge = SDIO_ClockEdge_Rising; SDIO_InitStructure.SDIO_ClockBypass = SDIO_ClockBypass_Disable; SDIO_InitStructure.SDIO_ClockPowerSave = SDIO_ClockPowerSave_Disable; SDIO_InitStructure.SDIO_BusWide = SDIO_BusWide_1b; SDIO_InitStructure.SDIO_HardwareFlowControl = SDIO_HardwareFlowControl_Disable; SDIO_Init(&SDIO_InitStructure);/* Set Power State to ON */
SDIO_SetPowerState(SDIO_PowerState_ON);/* Enable SDIO Clock */
SDIO_ClockCmd(ENABLE);/* CMD0: GO_IDLE_STATE -------------------------------------------------------*/
/* No CMD response required */ SDIO_CmdInitStructure.SDIO_Argument = 0x0; SDIO_CmdInitStructure.SDIO_CmdIndex = SDIO_GO_IDLE_STATE; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_No; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; // it will be TimeOut if i don't add this,It needs 74 clocks here //according to the SD spec // for( i = 0 ; i < 74 ; i++) { SDIO_SendCommand(&SDIO_CmdInitStructure); errorstatus = CmdError(); }if (errorstatus != SD_OK)
{ /* CMD Response TimeOut (wait for CMDSENT flag) */ return(errorstatus); }/* CMD8: SEND_IF_COND --------------------------------------------------------*/
/* Send CMD8 to verify SD card interface operating condition */ /* Argument: - [31:12]: Reserved (shall be set to '0') - [11:8]: Supply Voltage (VHS) 0x1 (Range: 2.7-3.6 V) - [7:0]: Check Pattern (recommended 0xAA) */ /* CMD Response: R7 */ SDIO_CmdInitStructure.SDIO_Argument = SD_CHECK_PATTERN; SDIO_CmdInitStructure.SDIO_CmdIndex = SDIO_SEND_IF_COND; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure);errorstatus = CmdResp7Error();
if (errorstatus == SD_OK)
{ CardType = SDIO_STD_CAPACITY_SD_CARD_V2_0; /* SD Card 2.0 */ SDType = SD_HIGH_CAPACITY; } else { /* CMD55 */ SDIO_CmdInitStructure.SDIO_Argument = 0x00; SDIO_CmdInitStructure.SDIO_CmdIndex = SDIO_APP_CMD; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure); errorstatus = CmdResp1Error(SDIO_APP_CMD); } /* CMD55 */ SDIO_CmdInitStructure.SDIO_Argument = 0x00; SDIO_CmdInitStructure.SDIO_CmdIndex = SDIO_APP_CMD; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure); errorstatus = CmdResp1Error(SDIO_APP_CMD);/* If errorstatus is Command TimeOut, it is a MMC card */
/* If errorstatus is SD_OK it is a SD card: SD card 2.0 (voltage range mismatch) or SD card 1.x */ if (errorstatus == SD_OK) { /* SD CARD */ /* Send ACMD41 SD_APP_OP_COND with Argument 0x80100000 */ while ((!validvoltage) && (count < SD_MAX_VOLT_TRIAL)) {/* SEND CMD55 APP_CMD with RCA as 0 */
SDIO_CmdInitStructure.SDIO_Argument = 0x00; SDIO_CmdInitStructure.SDIO_CmdIndex = SDIO_APP_CMD; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure);errorstatus = CmdResp1Error(SDIO_APP_CMD);
if (errorstatus != SD_OK)
{ return(errorstatus); } SDIO_CmdInitStructure.SDIO_Argument = SD_VOLTAGE_WINDOW_SD | SDType; SDIO_CmdInitStructure.SDIO_CmdIndex = SDIO_SD_APP_OP_COND; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure);errorstatus = CmdResp3Error();
if (errorstatus != SD_OK) { return(errorstatus); }response = SDIO_GetResponse(SDIO_RESP1);
validvoltage = (bool) (((response >> 31) == 1) ? 1 : 0); count++; } if (count >= SD_MAX_VOLT_TRIAL) { errorstatus = SD_INVALID_VOLTRANGE; return(errorstatus); }if (response &= SD_HIGH_CAPACITY)
{ CardType = SDIO_HIGH_CAPACITY_SD_CARD; }}/* else MMC Card */
return(errorstatus);
}- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2011-05-17 5:07 AM
//I cannot open the bbs this morning,Now it's ok.I can go on.
//In this function,It have be right since i add some code followed: static SD_Error FindSCR(uint16_t rca, uint32_t *pscr) { uint16_t delay_time = 0; uint32_t index = 0;/************************/
// uint32_t temp = 0, temp_go = 0; /************************/SD_Error errorstatus = SD_OK;
uint32_t tempscr[2] = {0, 0};/* Set Block Size To 8 Bytes */
/* Send CMD55 APP_CMD with argument as card's RCA */ SDIO_CmdInitStructure.SDIO_Argument = (uint32_t)8; SDIO_CmdInitStructure.SDIO_CmdIndex = SDIO_SET_BLOCKLEN; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure);errorstatus = CmdResp1Error(SDIO_SET_BLOCKLEN);
if (errorstatus != SD_OK)
{ return(errorstatus); }/* Send CMD55 APP_CMD with argument as card's RCA */
SDIO_CmdInitStructure.SDIO_Argument = (uint32_t) RCA << 16; SDIO_CmdInitStructure.SDIO_CmdIndex = SDIO_APP_CMD; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure);errorstatus = CmdResp1Error(SDIO_APP_CMD);
if (errorstatus != SD_OK)
{ return(errorstatus); } SDIO_DataInitStructure.SDIO_DataTimeOut = SD_DATATIMEOUT; SDIO_DataInitStructure.SDIO_DataLength = 8; SDIO_DataInitStructure.SDIO_DataBlockSize = SDIO_DataBlockSize_8b; SDIO_DataInitStructure.SDIO_TransferDir = SDIO_TransferDir_ToSDIO;SDIO_DataInitStructure.SDIO_TransferMode = SDIO_TransferMode_Block;
SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Enable;
SDIO_DataConfig(&SDIO_DataInitStructure);/************************/// It needs sometimes.
for(delay_time = 0 ; delay_time < 20 ;delay_time++)
{ __nop(); }/************************/
/* Send ACMD51 SD_APP_SEND_SCR with argument as 0 */
SDIO_CmdInitStructure.SDIO_Argument = 0x0; SDIO_CmdInitStructure.SDIO_CmdIndex = SDIO_SD_APP_SEND_SCR; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure);errorstatus = CmdResp1Error(SDIO_SD_APP_SEND_SCR);
if (errorstatus != SD_OK)
{ return(errorstatus); }/*******************************/
//temp = SDIO->STA;//清除STA标志�?,�?�测试用
//temp_go = temp + 1;/*******************************/
while (!(SDIO->STA & (SDIO_FLAG_RXOVERR | SDIO_FLAG_DCRCFAIL | SDIO_FLAG_DTIMEOUT | SDIO_FLAG_DBCKEND | SDIO_FLAG_STBITERR)))
{ if (SDIO_GetFlagStatus(SDIO_FLAG_RXDAVL) != RESET) { *(tempscr + index) = SDIO_ReadData(); index++;/*********************/// It need jump out. if(2 == index) { break; } /*********************/}
}if (SDIO_GetFlagStatus(SDIO_FLAG_DTIMEOUT) != RESET)
{ SDIO_ClearFlag(SDIO_FLAG_DTIMEOUT); errorstatus = SD_DATA_TIMEOUT; return(errorstatus); } else if (SDIO_GetFlagStatus(SDIO_FLAG_DCRCFAIL) != RESET) { SDIO_ClearFlag(SDIO_FLAG_DCRCFAIL); errorstatus = SD_DATA_CRC_FAIL; return(errorstatus); } else if (SDIO_GetFlagStatus(SDIO_FLAG_RXOVERR) != RESET) { SDIO_ClearFlag(SDIO_FLAG_RXOVERR); errorstatus = SD_RX_OVERRUN; return(errorstatus); } else if (SDIO_GetFlagStatus(SDIO_FLAG_STBITERR) != RESET) { SDIO_ClearFlag(SDIO_FLAG_STBITERR); errorstatus = SD_START_BIT_ERR; return(errorstatus); }/* Clear all the static flags */
SDIO_ClearFlag(SDIO_STATIC_FLAGS);*(pscr + 1) = ((tempscr[0] & SD_0TO7BITS) << 24) | ((tempscr[0] & SD_8TO15BITS) << 8) | ((tempscr[0] & SD_16TO23BITS) >> 8) | ((tempscr[0] & SD_24TO31BITS) >> 24);
*(pscr) = ((tempscr[1] & SD_0TO7BITS) << 24) | ((tempscr[1] & SD_8TO15BITS) << 8) | ((tempscr[1] & SD_16TO23BITS) >> 8) | ((tempscr[1] & SD_24TO31BITS) >> 24);
return(errorstatus);
}- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2011-05-17 5:07 AM
And i found some problems when i use the 2G SD_Card:
f_open( );f_write( );f_close(); ---->I must write this functions together,otherwise there will be some wrong data in the file.like this: Write_Something() { f_open( ...); f_write( ...); f_close(....); } It will be wrong if it be writed followed: Write_Something() { f_open( ...); delay(sometimes);//or do otherthings f_write( ...); delay(sometimes);//or do otherthings f_close(....); }- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2011-05-17 5:07 AM
Many e
ngineer
s in china said that they have various problems when using the ''SDIO+4bit+DMA''mode.''Some cards cannot R/W in this mode'',they said. So,most of them choose the ''SPI'' mode, But i cann't,I must solve this problem....