2012-04-16 1:16 PM
Hi all,
I am currently using the STM3210C evaluation board and have discovered something which is puzzling, and has to do with the clock frequencies. I am currently using Atollic to program the board and have initialised the micro by using the ''SystemInit()'' function and have determined that the following clock frequencies have been set by calling the ''RCC_GetClocksFreq()'' function:2012-04-16 2:51 PM
Wouldn't this simply be because SysTick clocks at 9 MHz? All of ST's references indicate that it clocks with HCLK / 8 by default, but can be HCLK. This is done no doubt because the counter is only 24-bits wide.
APB1 = PCLK1 APB2 = PCLK2 AHB = HCLK A TIMCLK derived from an APB1 clock of 36 MHz (72 DIV 2), will actually be 72 MHz as it won't be prescaled. Refer to the clock tree diagram. If you really believe there is a clocking problem, you should start by measuring the external oscillator (HSE), and also be exporting your internal clocks via MCO. If your serial ports work at the right baud rates, it would indicate the hardware and software are in agreement about what frequencies it's actually working with.2012-04-16 11:09 PM
Clive,
Thanks for your quick reply. I also thought that the SysTick clock is divided by 8 by I run ''SysTick_CLKSourceConfig( SysTick_CLKSource_HCLK )'' to ensure that the SysTick clock is set at 72 MHz; which as can be seen from my results it is not. This also does not explain why my TIMCLK is sitting at 8.61245 MHz? What could possibly be causing this? I will try your recommendations for checking to see if there is a clocking problem.2012-04-17 5:05 AM
You need to start by confirming what your input clocks are, and then that the PLL settings are correct.
You need to confirm if the external oscillator is actually 8 MHz, ST has some designs that use 25 MHz. You need to check the source, includes, IDE, or compiler command line to confirm what HSE_VALUE is set to, as it should match the input clock setting. Check also that the correct STM32F architecture has been selected. ie Connectivity vs Medium density or whatever. Alternatively you could HSI which should always be 8 MHz. If the PLL is run at overrated speeds (ie 25 * 9) the operation is probably undefined.2012-04-17 12:48 PM
Clive,
Again thanks for your suggestions, I will run through them and will let you know what I discover.2012-04-22 10:26 PM
I have managed to resolve the issue, once I checked through the code (and found nothing wrong), I discovered that the crystal on the board was wrong. The board is suppose to come with a 25 MHz crystal but for some weird reason I have a 6 MHz crystal. Once I accounted for this, my code is now working correctly.
I do however have another question which I was hoping could be cleared up. I know that if the APB prescaler is 1, that the peripheral timers runs at PCLK, other wise they run at 2 * PCLK. In my case the PCLK is set to 36 MHz, which is within the maximum specification given in the data sheet. What I would like to know is if it is okay/safe to have my peripheral timers running at 72 MHz (i.e. at 2*PCLK)?2012-04-23 6:42 AM
The Bus side of the timer would be running at 36 MHz, but the counter and internal logic are rated for 72 MHz operation, and running there. Having a high input frequency is helpful as it keeps the granularity small, allows a larger sampling rate for inputs, a counters the lameness of the the integer prescale. Still, in some circumstance you will need to run the part at sub-optimal speeds, or with ''magic number'' crystals in order to get the timers to generate specific frequencies. ie try getting 256 KHz out with a 72 MHz clock source.
2012-04-24 5:30 AM
Oh I see, thanks Clive for clearing that up.