2009-07-09 1:02 AM
STM32 use HSI clock source for USB operation.
2011-05-17 4:17 AM
Hi,
Code:
2.3.20 Universal serial bus (USB)
The STM32F103xx performance line embeds a USB device peripheral compatible with the USB full-speed 12 Mbs. The USB interface implements a full-speed (12 Mbit/s) function interface. It has software-configurable endpoint setting and suspend/resume support. The dedicated 48 MHz clock is generated from the internal main PLL (the clock source must use a HSE crystal oscillator).STM32F103x8/B Datasheet rev.10 page 17 so probably no, I think it's all about HSI accuracy, but you can always try :)2011-05-17 4:17 AM
Hi all,
I develop STM32 connect to PC via USB port. I want to made it low cost. Is it suitable to use HIS clock for USB operation ?. Thanks in advance. pichet :-] [ This message was edited by: pichetr22 on 09-07-2009 10:56 ]