cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 USB Virtual COM port driver Win7

morgan23
Associate
Posted on February 27, 2011 at 10:15

STM32 USB Virtual COM port driver Win7

8 REPLIES 8
ColdWeather
Senior
Posted on May 17, 2011 at 14:26

USB Communication Device Class (CDC), or Virtual COM Port, is a standart USB device class supported by any modern Windows without any additional user driver.

Plug and Play: as soon as the CDC/Virtual COMport demo is started and the ST board is connected via USB cable to the PC running Win7, the system recognizes the new device and shows it in the Device Manager.

greg_t
Associate II
Posted on May 17, 2011 at 14:26

It will not work with Windows 7

Posted on May 17, 2011 at 14:26

Hi ,

Could You please let me know and if possible to attach me the failing Screenshots.  It is quite strange that W7 is not working fine as we have already Certified it at Microsoft WHQL : either x86 and x64 versions.

Cheers,

STOne-32.

greg_t
Associate II
Posted on May 17, 2011 at 14:26

when connecting my board to PC with winXP the usb is recognized but when connected to win7 the usb is not recognized

Clifford1
Associate III
Posted on May 17, 2011 at 14:26

I have experienced problems with Windows 7 x64 using the x64 version of the driver.  Device Manager shows the device, but no connection can be made.

[edit]Further testing on Windows 7 32bit reveals the same problem. See Device Manager screen-shot below.  The target remains permanently stuck in the USB interrupt context.  The target in this case is an STM32F105VC (connectivity line)

0690X00000604vfQAA.png

Clifford1
Associate III
Posted on May 17, 2011 at 14:26

I appear to have fixed this issue, it was a problem with the target device implementation not the driver.

My implementation modifies the rather basic example VCP code to make it more general, to have the same API as my USAT driver, and to integrate it with Keil RTX RTOS kernel.  Getting that right was key to the port being correctly recognised it seems; though it was working on XP.

It is a shame that the example code is so specialised and poorly documented that adapting it for one's own needs risks breaking it.

Clifford1
Associate III
Posted on May 17, 2011 at 14:26

I appear to have fixed this issue, it was a problem with the target device implementation not the driver.

My implementation modifies the rather basic example VCP code to make it more general, to have the same API as my USAT driver, and to integrate it with Keil RTX RTOS kernel.  Getting that right was key to the port being correctly recognised it seems; though it was working on XP.

It is a shame that the example code is so specialised and poorly documented that adapting it for one's own needs risks breaking it.