2008-06-14 6:59 PM
STM32-SK Kickstart run from flash
2011-05-17 3:37 AM
If you have the latest version EWARM5.11A installed, you can find under:
IAR Systems\Embedded Workbench 5.0\ARM\examples\ST\STM32F10x\STM32-Eval pre-configured examples for both RAM and Flash.2011-05-17 3:37 AM
Hi-
I recently received the IAR STM32-SK dev kit. The examples run properly from RAM but I'd like to load and run them from flash now (no JLink connected). How should I reconfigure the project to build for flash execution? How do I download the built program to flash? Thanks, John Speth.2011-05-17 3:37 AM
Hi john,
Please refer to topic ''run from flash'' posted by suyongyao. Accidentally created another topic instead of replying you.2011-05-17 3:37 AM
Quote:
Please refer to topic ''run from flash'' posted by suyongyao.