cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 RS485通讯 - 在2.5Mbps波特率下可以接收数据吗?

caixf
Associate

STM32F051C8T6产品,想用来和多摩川的编码器产品通讯,发送数据0x02,多摩川编码器发送6个字节返回。但用6个字节的中断得不到数据,用6个字节读取也无法得到数据。中断只能收到一个字节,02。有指导问题出在哪里了?

1 REPLY 1
Lina_DABASINSKAITE
Community manager
Community manager

TRANSLATION: 
STM32 RS485 Communication - Can I receive data at 2.5Mbps baud rate?

STM32F051C8T6 product, I want to use it to communicate with Tamagawa's encoder product, send data 0x02, Tamagawa encoder sends 6 bytes back. But I can't get data with 6 bytes interrupt, and I can't get data with 6 bytes read. The interrupt can only receive a byte, 02. there is a guide to where the problem is?


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.