cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Primer2 - st-link functionality

Posted on January 04, 2018 at 23:25

Just playing with STM32 Primer2 (quite old hardware:

http://www.stm32circle.com/resources/stm32primer2.php

 ) and have a question related to the debugger interface.

This piece of hw uses rlink interface for Ride7 IDE to debug/program the target MCU. The ST72651AR6T1 MCU (32k flash)  handles this task (i.e. it steers the SWD pins of the target MCU).

I would like to use the Primer2 with Keil but Keil does not support the rlink (at least I cannot make it use rlink). I wonder if someone solved this problem - ideally I would need st-link firmware for ST72651AR6T1. MAybe there isa another way of solving this problem...

Thanks,

Bogdan

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on January 05, 2018 at 07:47

Of course I can do some changes on the PCB and connect external programmer but I am looking for less invasive solution...

Andrew Neil
Super User
Posted on January 05, 2018 at 09:27

RLink and the 

STM32 Primer2

  are Raisonance products - so you should contact Raisonance for support 

http://www.raisonance.com/raisonance-support.html

 

As Raisonance is a competitor for Keil, it's not surprising that the RLink isn't supported in Keil!

A genuine ST-Link is only ~$20; Chinese imitations are just a couple of dollars.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on January 05, 2018 at 11:27

I know, I know, I know...

I purposely mentioned ST7 as it's ST product. Also the target MCU i.e. STMF107 is a ST product. That's why I posted the topic here. I believe it's right place where experienced people share theirs ideas and concerns....

I already mentioned that I can hack the PCB and connect external programmer and looking for an alternative, more subtle way to achieve the same goal.