cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 PMSM foc sdk 5.0 serial communication

Jiaxing Wang
Associate
Posted on April 05, 2018 at 04:11

I am working with stm32 PMSM foc sdk 5.0. I want to drive the system by the application board and it can send a command to the motor drive board and get a feedback.The application board and motor drive board communicate using a serial communication. I was wondering if there is a demo that I can refer to.

0 REPLIES 0