2013-07-09 9:10 PM
STM32 embedded target for MATLAB and Simulink does not work with latest Matlab R2013a release (as it was supposed to work only with previous R2012b release)
Any one had better experience with R2013a? Are there any known issues that has been resolved (or needs to be resolved) with this STM32 Support Package for Matlab? Are there any updates? Thanks! #stm32-mat/target #stm32-mat/target-matlab2013-07-10 8:28 AM
2013-07-10 11:51 AM
Hello Mr.Pascal,
Here's a brief description of my testing : I use Windows-7 (64-bit O.S) and testing with Matlab R2013a and IAR tool chain. The model is a very simple model to just blink an LED on the STM32F4 Discovery board. (though STM's Support Package demo used STM32 Eval board, it's a simple matter to toggle an LED on a Discovery Board once we know what pins to use) GPIOD pin 15 is configured to toggle the LED so there are just two model blocks : GPIOD_Config (with pin15 enabled as output) and GPIO_Write (with GPIOD pin15 selected to toggle) All the Simulink Configuration Parameters are properly set as per the STM's Support Package documentation to just check models and compile them. Simulink/RealTime Workshop gives many errors related to models and the libraries (even before it invokes the IAR compiler tools). Running Simulink Model Advisor gives many warnings due to changes in Simulink tools for R2013 and even after resolving most of these there are many issues which Simulink complains may be due to changes in tools interfaces etc. Few of the errors I get (eventhough the model is in the library and is placed on the editor and properly configured): Error in S-function 'STM32_DiscBrd_BlinkBlueLed/GPIOD_Config': S-Function 'GPIOD_Config' does not exist Error in S-function 'STM32_DiscBrd_BlinkBlueLed/GPIO_Write': S-Function 'GPIO_Write' does not exist Recreating this simple model and compiling it on Matlab R2013a by STM team will highlight all these and help to fix them. Thanks, Best Regards, Anbazhagan2013-07-11 1:36 AM
Hello Mr Anbazhagan,
Unfortunately only mex32 files are provided. It can't work with 64bit OS you are using. I hope we will be able to provide both mex32 and mex64 files for September release. Best regards Pascal2013-07-11 10:37 AM
Hi Pascal,
Good to know that the issue is due to non-support of Windows 64-bit O.S (but the support package documentation does n't mention it). Hope the support will be extended to 64-bit O.S soon since multicore CPUs and 64-bit O.S are the hot technologies currently in use everywhere. Thanks, Best regards, Anbazhagan2013-07-22 3:30 PM
Hello
:)I'm using
Matlab
2012B
with
STM32-MAT/TARGET
(
Win732bit)
.Where
in the example
''
BlinkBlueLed'' or ''
BlinkGreenLed''can I
change the time
/ frequency of
LED blinking
?Regards
2013-08-14 6:39 AM
Hello guys.
I am having problem performing processor in the loop simulation with the STM32F Discovery board. I am trying to load the example 'Filtrage_PIL_Int32.mdl' that comes with the STM32F embedded target for matlab. I get the following error when I compile the code generated from the 'Filtrage_int32.mdl': ### Wrapping unrecognized make command (angle brackets added) ### <''%MATLAB%\bin\%MATLAB_WIN_VER%\gmake''> ### in default batch file ###Makefile for KEIL ###BuildMode : real_time ### Successfully compiled source main.c ### Successfully compiled source Filtrage_int32.c ''### BUILD_MODE real_time'' Error: L6218E: Undefined symbol profileTimerInit (referred from main.o). Error: L6218E: Undefined symbol xilInit (referred from main.o). Error: L6218E: Undefined symbol xilRun (referred from main.o). Finished: 0 information, 0 warning and 3 error messages. gmake: *** [Filtrage_int32.axf] Error 12013-08-28 7:32 AM
2013-08-28 7:37 AM
Hello Guys.
I managed to get my problem solved. I was trying to build the secondary model separately.2013-09-01 8:36 PM
hello Mr.
when you test the demo,have you seen the probelm like this: Warning: ### IAR toolchain not automatically found. > In getToolPath at 36 In stm32F4xx_PostApplyCallback at 17 In F:\MATLAB\R2012b\toolbox\rtw\rtw\private\stfTargetActivateCB.p>loc_eval at 44 In F:\MATLAB\R2012b\toolbox\rtw\rtw\private\stfTargetActivateCB.p>stfTargetActivateCB at 17 In rtwprivate at 16 In F:\MATLAB\R2012b\toolbox\simulink\simulink\private\configDlgAction.p>configDlgAction at 191 In slprivate at 12 matlab 2012b(win7 32bits) I don't know how to solve it,I configure the simulink with the readme file.I don't know what the wrong is.If you have free time,please help me.and I think you can write a course to show how you configure the simulink,thanks.