2021-04-07 05:27 AM
Hi,
I was able to generate code for an STM32G474 with Matlab/Simulink 2020b. After an update to Matlab/Simulink 2021a code generation is no more possible. The only STM device I can choose is "ST10/Super10".
What can I do or when will a fix be available?
Thanks for help!
Thorsten
Solved! Go to Solution.
2021-04-15 12:29 AM
I am afraid that you are out of luck. STM32-MAT/TARGET is NRND (Not Recommended for New Design), and the last version, 5.6.0, is only recommended for Matlab R2018b. I already moved to other vendors' MCUs.
2021-04-15 12:29 AM
I am afraid that you are out of luck. STM32-MAT/TARGET is NRND (Not Recommended for New Design), and the last version, 5.6.0, is only recommended for Matlab R2018b. I already moved to other vendors' MCUs.
2021-05-30 10:35 PM
Whether to use rtwbuild (model)
There is a build button when opening Embedded Coder from the Apps tab on the Simulink model